This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828-EP: MIN/MAX datasheet values, design margin.

Part Number: LMK04828-EP

Hi team, 

I'm working with a customer that is potentially interested in LMK04828-EP. Could you please help with the questions below: 

Re: the datasheet parameter table on page 8, can you confirm that the max/min parameters are guaranteed over 3.15V < Vcc < 3.45V,  -55C to 105C. 

In our case the frequency of VCO0 is 2457MHz which is very close to the lower limit of the VCO0 for LMK04828-EP, do you have any concerns using the device so close to the VCO0 Min over -55C to 105C? 

Thanks in advance 

Dan