Part Number: CDCLVD1213
Hi team,
Customer want LVCMOS in LVDS out translator. Can CDCLVD1213 support this?
In the datasheet it says "The input can either be LVDS, LVPECL, or CML".
If not, please suggest one device, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCLVD1213
Hi team,
Customer want LVCMOS in LVDS out translator. Can CDCLVD1213 support this?
In the datasheet it says "The input can either be LVDS, LVPECL, or CML".
If not, please suggest one device, thanks.
You could use a single-ended input. The input must meet the input requirements in datasheet table 6.5. Simply input the LVCMOS signal to one of the differential input, and bias the other pin to the common of the the LVCMOS signal.
For example, you can input a 1.6Vpp LVCMOS signal to INP. Bias INN to 1.25V (assuming the LVCMOS clock swings from 450mV to 2.05V).
Kind regards,
Lane