Part Number: LMK00105
Hi team,
My customer considers to use LMK00105 and provided some questions.
- They considers to use 3.3V CMOS single-ended output crystal oscillator (slew rate of about 0.3V / ns) as a clock source.
In this case, they should connect it to CLKin pin.
Is this understanding correct? - In “8.1.1 Clock Inputs” of the LMK00105 Datasheet, a 50Ω terminated example is described.
However, max output current of 3.3V CMOS crystal oscillator only has ±4mA.
What should they do in this case?
I'm looking forward to hearing back from you.
Best regards,
Shota Mago