Part Number: LMX2594
Team,
My customer has the following question.
The issue I’m having is a long tune time at the VCO band breaks around 12 GHz (around 600 us) and 13.9 GHz (around 300 us). This occurs for tunes from one VCO to another. I am using the recommended settings as follows below from the datasheet.
Between 11.9 and 12.1 GHz
VCO_SEL = 4
VCO_DACISET_STRT = 300
VCO_CAPCTRL_STRT = 1
Everywhere else
VCO_SEL = 7
VCO_DACISET_STRT = 300
VCO_CAPCTRL_STRT = 183
If I set the QUICK_RECAL_EN bit high, then the tune time drops to around 300 us for 12 GHz and around 50 us for 13.9 GHz. I read in the datasheet that QUICK_RECAL_EN shouldn’t be done between 11.9 and 12.1 GHz. Can you provide more information about that? That bit is the only way I have found to speed things up. Maybe you have some other suggestions for me to try to speed up those spots.
Regards,
Aaron