Part Number: CDCM9102
When OS1=1 and OS2=2, OSCOUT is enabled in LVPECL mode. In this case, what is the performance (Duty, Jiter and so on) of the clock signal from OSCOUT pin?
Thanks
Tamio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCM9102
When OS1=1 and OS2=2, OSCOUT is enabled in LVPECL mode. In this case, what is the performance (Duty, Jiter and so on) of the clock signal from OSCOUT pin?
Thanks
Tamio
Hi, Hao,
Thank you for supporting.
According to the following Table 3, to be enabled OSCOUT, OS1 and OS2 must to be configured to 1 and 1, but the clock output is configured to LVPECL mode. If the clock output is configured to LVCMOS mode or LVDS mode, OSCOUT can not use. Is this understanding correct?
As for the performance of OSCOUT, which item in list 7.5 and 7.6 should I confirm? Please clarify the item I should confirm.
7.5 Electrical Characteristics
7.6 Timing Requirements
Thanks
Tamio
Hi, Hao,
Is your meaning that the jitter specification of OSCOUT pin is depending on the OUTPUT mode selected by OS1 and OS2? And, is the AC specification also depending on the OUTPUT mode?
Please show it clarify.
Thanks
Tamio
No I meant OUT0 and OUT1. I'm afraid that the additive jitter of the buffer for OSCOUT is not available.
Regards,
Hao
Hi, Hao,
I want to know the specification of OSCOUT pin as shown the following figure
The only thing I understood is that OSCOUT is the output of LVCMOS. As for the specification of OSCOUT pin, I can't understand any more even if I checked the other device (CDCM6xxx series).
Is there any specification for OSCOUT pin?
Thanks
Tamio
Hi Tamio,
I'm afraid we don't have any spec for OSCOUT output. It's a simple LVCMOS buffer for the input and we don't expect it to be used as high performance clock source.
Regards,
Hao