This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2492: FMCW and integer boundaries

Part Number: LMX2492


Hi,

I want to perform a linear FMCW sweep from 13.4 to 14.0 GHz using a 100 MHz reference (I can change the XO frequency if you have another recommendation).

When performing such a wide sweep across 5 integer boundaries can I expect LMX2492 to maintain a "clean sweep" without any RF phase or amplitude discontinuities near the boundaries? This is critical for proper FMCW operation.

Related to this, I also read somewhere on this forum that the fractional counter can only "roll over 8 times". I guess that means one can only sweep across 8 integer boundaries? Are there other such limitations/considerations I should know about?

Thanks!

Christer