Part Number: LMK00308
Other Parts Discussed in Thread: LMK05318
Hello,
At the Clock Inputs there is a slow Clock Signal (<10MHz). Switching from one to the other Input is done when both Clock Signals are "low".
Then, switching from CLKin0 to CLKin1 and back generates an short (10ns ... 20ns) "high-pulse" at the Outputs.
Is this a known behavior? We can reproduce this bahavior with an LMK00308EVAL board.
I could not find any informations in the datasheet concerning the timing behavior of the switching function.
Propagation Delay? Glitchfree? Drift? Time until Output Signal is valid...