This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04803: LMK04803B output question

Part Number: LMK04803


hello Team

If the input is 200Mhz, can LMK04803B output 200Mhz ? How to setup? the customer try to output this frequecy but not output the right .

  • Hello,

    Yes, this is possible if the VCO2 is tuned to a multiple of 200 MHz and the output divider is set correctly such as 2 GHz divide by 10.

    To use in dual loop mode, the VCXO must also be an integer divide ratio of 200MHz input.

    The TICS Pro GUI can be used to setup the device configuration.

    Regards,

    Liam