This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572: Sub-Fractional Spurs

Part Number: LMX2572

Hi Team,

My customer is evaluating LMX2572 on their ES board, and they have a question about sub-fractional spurs.
When they evaluated the 2nd  ES board, sub-fractional spurs of LMX2572 became around 5dB higher than that of the 1st ES board.
They do not change application of LMX2572 and settings, they also use MASH_SEED with the same setting.
It is a general question,
Q1: Does the sub-fractional spurs vary by variation of LMX2572 characteristic, part to part, or lot to lot?

Thank you.

Best Regards,

Koshi Ninomiya

  • Hi Ninomiya-san,

    Do you have their configuration such as phase detector frequency, VCO frequency, etc?

  • Hi Fung-san,

    Their configuration is as follows,

    Option-1: 5523MHz_190315.txt

    R78	0x4E0001
    R75	0x4B0800
    R71	0x470081
    R57	0x390020
    R46	0x2E07F1
    R45	0x2DCE1E
    R44	0x2C3F23
    R43	0x2B0017
    R42	0x2A0000
    R41	0x290051
    R40	0x280000
    R39	0x270064
    R38	0x260000
    R37	0x258305
    R36	0x240037
    R34	0x220010
    R30	0x1E18A6
    R29	0x1D0000
    R14	0x0E1878
    R12	0x0C5001
    R11	0x0BB018
    R10	0x0A10F8
    R9	0x091004
    R0	0x00231C
    

    Option-2:5629r25MHz_190315.txt

    R78	0x4E0001
    R75	0x4B0800
    R71	0x470081
    R57	0x390020
    R46	0x2E07F1
    R45	0x2DCE1E
    R44	0x2C3F23
    R43	0x2B0075
    R42	0x2A0000
    R41	0x290111
    R40	0x280000
    R39	0x270190
    R38	0x260000
    R37	0x258305
    R36	0x240038
    R34	0x220010
    R30	0x1E18A6
    R29	0x1D0000
    R14	0x0E1878
    R12	0x0C5001
    R11	0x0BB018
    R10	0x0A10F8
    R9	0x091004
    R0	0x00231C
    

    Thank you.

    Best Regards,

    Koshi Ninomiya

  • Hi Ninomiya-san,

    in Option 1, are you referring to 1MHz and 500kHz spurs?

    In Option 2, 250kHz and 125kHz spurs?

    In both cases, you can set the fractional DEN to an irrational number such as 400001234 to eliminate these spurs.