Other Parts Discussed in Thread: CLOCKTREETOOL
OS is windows 10, Install java 1.8.0_231, download CTT-Automotive-v1.0.0.8, and install.
After install, right click of CTT-Automotive-v1.0.0.7.jar,
On CTT UI, can't select any device.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CLOCKTREETOOL
OS is windows 10, Install java 1.8.0_231, download CTT-Automotive-v1.0.0.8, and install.
After install, right click of CTT-Automotive-v1.0.0.7.jar,
On CTT UI, can't select any device.
In your installation folder do you have "XMLFiles" folder? This usually happens when the install manager does not unpack all necessary folders in the destination directory. Make sure you install the tool in a directory where you have a RW access (like on the desktop or something).
Hope it helps,
Alex
Can you try the attached package instead? I wonder if the download from ti.com site doesn't work for you.
thanks,
Alex
Hello again,
It's been a day or so with no response. Did you have a chance to try the attached file?
thanks,
Alex
Hi Alex
The attached file is same as I used before. I compared by beyond compare.
Hello,
Again this has to be something wrong with the way your system sees these xmls. Could that be the chinese encoding? Can you do this for me please. Open a command line and do
java -jar <CTT path to jar>/<jar file>
then send me the error message?
thanks,
Alex
Thank you Alex
It's OK when go to CTT path first, then start jar file.
The command is:
cd <CTT path to jar>
java -jar CTT-Automotive-v1.0.0.8.jar
Then can select divice.
java -jar <CTT path to jar>/<jar file>, is not OK
The release is search device_SR.xml in current directory.
C:\Users\fengjiang>java -jar C:\ti_ctt\TI_Clock_Tree_Tool\CTT-Automotive-v1.0.0.8\CTT-Automotive-v1.0.0.8.jar
java.io.FileNotFoundException: C:\Users\fengjiang\XMLFiles\device_SR.xml (系统找不到指定的路径。)
java.io.FileNotFoundException: C:\Users\fengjiang\XMLFiles\device_SR.xml (系统找不到指定的路径。)
at java.io.FileInputStream.open0(Native Method)
at java.io.FileInputStream.open(Unknown Source)
at java.io.FileInputStream.<init>(Unknown Source)
at java.io.FileInputStream.<init>(Unknown Source)
at sun.net.www.protocol.file.FileURLConnection.connect(Unknown Source)
at sun.net.www.protocol.file.FileURLConnection.getInputStream(Unknown Source)
at com.sun.org.apache.xerces.internal.impl.XMLEntityManager.setupCurrentEntity(Unknown Source)
at com.sun.org.apache.xerces.internal.impl.XMLVersionDetector.determineDocVersion(Unknown Source)
at com.sun.org.apache.xerces.internal.parsers.XML11Configuration.parse(Unknown Source)
at com.sun.org.apache.xerces.internal.parsers.XML11Configuration.parse(Unknown Source)
at com.sun.org.apache.xerces.internal.parsers.XMLParser.parse(Unknown Source)
at com.sun.org.apache.xerces.internal.parsers.DOMParser.parse(Unknown Source)
at org.ti.clockTreeTool.SiliconRevision_XMLParser.ParserSiliconRevision_XML.parseXMLFile(ParserSiliconRevision_XML.java:44)
at org.ti.clockTreeTool.SiliconRevision_XMLParser.ParserSiliconRevision_XML.<init>(ParserSiliconRevision_XML.java:34)
at org.ti.clockTreeTool.infoScreen.checkDev.prepareGUI(checkDev.java:102)
at org.ti.clockTreeTool.infoScreen.checkDev.<init>(checkDev.java:45)
at org.ti.clockTreeTool.simulation.ClockTreeTool.main(ClockTreeTool.java:85)
That's OK, this didn't work for me either, so you are right, CD first into the install folder where the jar is located and then do just "java -jar CTT-Automotive-v1.0.0.8.jar".
So this worked for you. Please mark this post as resolved.
However, I want to make sure the issue is not happening for other users as well. How do you run jar outside the console? You said you right-click and then what do you select?
thanks,
Alex