This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: OSCin doubler function

Part Number: LMX2595

Hi team,

My customer is using TI's LMX2595 series PLL. During the use, it is found that the loop characteristics of enabling and disabling OSC_2x are different.

When FOSC = 100MHz, osc_2x = 2x, FPD = 200MHz, the loop characteristics are shown in Figure 1;

Set FOSC = 200MHz, osc_2x = 1X, FPD = 200MHz, and the loop characteristics are shown in Figure 2.

The FPD frequency set in these two cases is the same. When the spectrometer is adjusted to span = 500KHz, it can be seen that the loop using the oscin doubler function drops smoothly; the loop without the oscin doubler function will have obvious depression. Judging from the function of oscin doubler, it can improve phase noise, but is the phase noise performance better in Figure 2 (osc_2x = 1x)? Why is that

Figure 1 FOSC = 100MHz, osc_2x = 2x, FPD = 200MHz

Figure 2  FOSC = 200MHz, osc_2x = 1X, FPD = 200MHz

Best Regards,
Amy Luo

  • Hi Amy,

    Where is the 100MHz and 200MHz reference clock came from? Are their phase noise good?

    I expect the phase noise should be same with or without the doubler. 

    Figure 2 doesn't look right.  How does it look if the doubler is enabled using the same spectrum analyzer setting?