Hi,
I'm not familiar with XTAL osc circuits.
Using the TICS Pro software, I don't seem to be able to use a Crystal with Load Capacitance requirement of 18pf.
I set Cstray to 4.5pf, CL ext to 0pf and CL to 18pf. Software errors.
Questions:
1/. What do I need to do to make an ABM3C-25.000MHZ-D4Y-T work with the CDCI6214?
https://abracon.com/Resonators/abm3c.pdf
2/. Should I use a different 25M XTAL with 50ppm? If so, can you recommend one and tell me what numbers to program into the CDCI6214.
Thanks
Dave S