Hello,
Related to the 12pF specification listed in the datasheet, is it OK to use a crystal with 6pF load capacitance or is a 12pF +/- 10% crystal required?
To be specific - can I use either:
EPSON TIMING: MC-306 32.7680K-A:ROHS (12.5pF)
or:
EPSON TIMING: MC-306 32.7680K-E3:ROHS (6pF).
Thanks
Uri