Part Number: LMK04616
Other Parts Discussed in Thread: USB2ANY
Hi,
Is it possible to configure an LMK04616 device implemented on a custom board (not an EVM) through USB2ANY dongle and TICS Pro software ?
Thanks in advance for your help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Cedric,
Yes, it is possible. The most straightforward method is copying the USB2ANY header pinout and connections directly from the EVM onto your new design. If the GPIO pin control features like pin SYNC or RESET are not needed, the header connections could also be reduced to just the SPI lines.
Regards,