Part Number: CDCE6214-Q1
Other Parts Discussed in Thread: CDCI6214, CDCE6214
Hi,
What is formula to get output frequency of CDCE6214 based on PLL configuration. Is it similar to formula given on CDCI6214 datashet page 94.
Thanks,
Akshay
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCE6214-Q1
Other Parts Discussed in Thread: CDCI6214, CDCE6214
Hi,
What is formula to get output frequency of CDCE6214 based on PLL configuration. Is it similar to formula given on CDCI6214 datashet page 94.
Thanks,
Akshay
Hello Akshay,
It is just common PLL frequency calculation: f_VCO = PFD * (N + NUM / DEN), and f_out = f_VCO / PS / CH_DIV. Where f_VCO is VCO frequency; PFD is Phase Frequency Detector frequency; N is feedback N divider; NUM is numerator of fractional feedback divider and DEN is denominator; f_out is output frequency; PS is prescalar (first stage divider after VCO); CH_DIV is channel divider.
I recommend downloading Ticspro to understand how the device works. http://www.ti.com/tool/TICSPRO-SW
Regards,
Hao
Hi Hao,
Thanks for frequency calculations. I am trying to generate 2.3203125 MHz frequency from 74.25 MHz oscillator.
I configured registers as below:
ip_rdiv = 2, So f_PFD = 37.125
PLL_NC = 65, PLL_NUM = 5, PLL_DEN = 1, So f_VCO = 2598.75 MHz
PLL_PSA = 1, ch1_iod_div = 224
Using above configuration expected output frequency is 2.3203125 MHz but I am getting 2.18772 MHz at output. Please help why there is difference in frequency? Frequency also changes by changing MASH_ORDER value.
Is there version of Ticspro that works on linux platform?
Thanks,
Akshay
Hi Akshay,
No we don't have a linux version of Ticspro. Please check two things.
1. Make sure to either write a '1' to bit "recal" R0[4] or a bit to bit "swrst" R0[2] after changing the frequency setting. The former is VCO re-calibration and the latter is software reset. Both can initiate VCO re-calibration.
2. Read back bit "lock_det" R7[0] to make sure that the PLL is locked.
Regards,
Hao
Also, PSA only be 4, 5 or 6. Check out the latest programming manual: http://www.ti.com/lit/ug/snau247b/snau247b.pdf
Regards,
Hao
I done VCO re-calibration and read back bit "lock_det" R7[0], value of R7[0] = 1. Still not getting required frequency.
I set register bits PLL_PSA = 1 ( PSA value = 5).
Using N + (NUM / DEN) equation.
Thanks,
Akshay
Hi Akshay,
Are you still using N = 65, PLL_NUM = 5, PLL_DEN = 1?
It should be N = 70, PLL_NUM = 0 and PLL_DEN = 1.
Regards,
Hao
Hi Hao,
I got required frequency using N = 70, PLL_NUM = 0 and PLL_DEN = 1.
But according to formula N = 65, PLL_NUM = 5, PLL_DEN = 1 OR N = 65, PLL_NUM = 10, PLL_DEN = 2 should also give required frequency. By making PLL_NUM = 0, we are making (NUM/DEN) factor 0. What is use of PLL_NUM and PLL_DEN.
Thanks
Akshay
Hi Akshay,
PLL_NUM is the numerator of PLL fractional feedback divider and PLL_DEN is the denominator. N is the integer part of the divider. So for example, with a divider ratio of 6144/125, N = floor(6144/125) = 49. NUM = 6144 mod 125 = 19. DEN = 125.
In your case since you are using integer mode, you can simply set NUM = 0 and DEN = 1.
Regards,
Hao
Hi,
Thanks for explanation.
Is Integer mode or fractional mode is decided using MASH_ORDER bit of R27 Register? I am using MASH_ORDER = 2. What is meaning of 1st Order, 2nd Order and 3rd Order Modulator and how it affect ouptut?
Thanks,
Akshay
Hello Akshay,
If the fractional PLL is not used then the fractional order (MASH order) can be set to integer mode, in this case R27[1:0] can be set to 0.
Regards,
Hao