Hi,
I am using the LMX2594 to generate a single constant frequency.
I have some questions regarding the recommended initial power-up sequence (datasheet 7.5.1 paragraph):
1) in step 4: "Program registers as shown in the register map in REVERSE order from highest to lowest.":
Should I program register R0 in this step as well (in addition to programming it in step 6) ?
2) Register R0 is being programmed in steps 2,3,(4?), and 6. Should I program it with FCAL_EN='1' only in step 6?
Best regards,
Vadim.