Other Parts Discussed in Thread: USB2ANY
Hi,
We are currently starting up a PCB equipped with LMX 2594.
I have two questions.
First, when I turn on the power and read back with SPI, all registers return 0x0000.
Although page 39 of the datasheet explains that this device has a power-on reset feature, I am confused because it does not appear to work.
This happens every time the power is turned on.
Second, the software reset sometimes feels like it doesn't work.
We use an oscilloscope to verify that the SPI communication from our equipment to this device meets the timing specifications described in the data sheet. The program is executed according to the program sequence described in the data sheet. However, even if all register settings are completed, the set frequency is not obtained and the register readback is 0x0000.
This means that the condition mentioned in the first question, that all registers appear to be set to 0x0000 after power on, has not been resolved after the soft reset.
This doesn't happen all the time, and it happens occasionally, so I don't know how to deal with it.
Is there any knowledge that could be helpful?