This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04208: LMK04208 configuration

Part Number: LMK04208

Hi Team,

One of my customer is using LMK04208 for ZCU111 Xilinx RFSoC. The output Clock frequencies required is as below.

  1. OUT0 -> 7.68 MHz
  2. OUT1 -> 7.68 MHz
  3. OUT2 -> 245.76 MHz
  4. OUT3 -> 491.52 MHz
  5. OUT4 -> 491.52 MHz

 The inputs:

CLKIN0 -> 122.88 MHz

CLKIN1 -> terminated in connector 

Customer requirement is: Feed 10MHz to CLKIN1. Do not use CLKIN0.

Customer have arrived on the values for the configuration they require. Can you please review/validate the attached configuration?

Regards, Shinu Mathew. 

  • Configuration file attached.

    PLL_Config.tcs

    Thanks, Shinu Mathew. 

  • Hello Team,

    Can you please help on this.

    Regards, Shinu Mathew.

  • Hi Team,

    Can you please help on this request.

    Regards, Shinu Mathew

  • The configuration has some problem for 0-delay feedback. Please clarify what's the synchronization requirement for 10 MHz input and other outputs.

    Normally, we will adopt the lowest output frequency as the feedback clock, then other higher frequency clocks (= n * feedback clock, n is an integer) can be aligned on the same rising edges.

  • Hi Shawn,

    "Please clarify what's the synchronization requirement for 10 MHz input and other outputs”.

    Not Sure what inputs you need for above point. Are you asking about the stratum level? Customer indeed want all the outputs to be synchronized to the inputs. Inputs are 12.8MHz and 10MHz. Output requirements are shared already. 

    Customer tried the attached configuration, 0-delay and dividers are fine. 

    However, they have trouble performing “switching between two clock inputs”.

    When the other CLK (CLKIN0) is enabled, the PLL1 does not lock. PLL1 locks when only one of the clocks are enabled. Please note the R-divider is kept same for both inputs as recommended.

    Please help to close this as early as possible.

    Regards, Shinu. 

  • 1, Input the correct clocks for CLKin0 and CLKin1, find the Greatest Common Divisor (GCD) frequency for CLKin0 and CLKin1, which could be used for PLL1 phase detect frequency. Set CLKin Dividers and R divider for CLKin0 and CLKin1, if different CLKin Dividers can't get the same output frequency, then we need change R divider when switching to another CLKin.


    2, Feedback clock: Select the lowest output frequency in all outputs need to be synchronized. Here 7.68 MHz may be your preferred.


    3, Set N divider for PLL1 to achieve the same frequency as R divider path.

  • Hi Shawn,

    Thanks for the feedback.

    Please find the attach file shared by customer can you please check and comment.

    10M_CLKIN1_CLKIN0-DIS-NO-delay-Auto-CLKIN1-PLL1.tcs

    R0 (INIT)	0x00160040
    R0	0x00143000
    R1	0x00143001
    R2	0x00140182
    R3	0x001400C3
    R4	0x001400C4
    R5	0x001400C5
    R6	0x01400006
    R7	0x04400007
    R8	0x04010008
    R9	0x55555549
    R10	0x910249AA
    R11	0x1401100B
    R12	0x1B0C006C
    R13	0x2302884D
    R14	0x0230000E
    R15	0x8000800F
    R16	0xC1550410
    R24	0x00000058
    R25	0x02C9C419
    R26	0xAFA8001A
    R27	0x10001F5B
    R28	0x0026001C
    R29	0x0180019D
    R30	0x0200019E
    R31	0x003F001F
    

    Regards, Shinu.

  • Hi Shawn,

    Thanks for the feedback.

    Please find the attach file shared by customer can you please check and comment.

    3704.10M_CLKIN1_CLKIN0-DIS-NO-delay-Auto-CLKIN1-PLL1.tcs

    R0 (INIT)	0x00160040
    R0	0x00143000
    R1	0x00143001
    R2	0x00140182
    R3	0x001400C3
    R4	0x001400C4
    R5	0x001400C5
    R6	0x01400006
    R7	0x04400007
    R8	0x04010008
    R9	0x55555549
    R10	0x910249AA
    R11	0x1401100B
    R12	0x1B0C006C
    R13	0x2302884D
    R14	0x0230000E
    R15	0x8000800F
    R16	0xC1550410
    R24	0x00000058
    R25	0x02C9C419
    R26	0xAFA8001A
    R27	0x10001F5B
    R28	0x0026001C
    R29	0x0180019D
    R30	0x0200019E
    R31	0x003F001F
    

    Regards, Shinu.

  • It can work, but why do not use CLKin0 or CLKin1 7.68 MHz as feedback clock ?

  • Hi Shawn,

    You suggested CLKIN0 or IN1 to br 7.68MHz? If yes, it is not possible. It has to be 12.8M (IN0) and 10M (IN1).

    Or want CLKOUT0, CLKOUT1 as feedback clock?

    Can you please clarify.

    Regards, Shinu Mathew. 

  • 10M_CLKIN1_12M8_CLKIN0-NO-delay-PLL1-40kHz_PDF1-CLKout0_FB-1p6mA_CP1-PLL1WND_40ns.tcs

    Here is an example.

    1, Calculate GCD for 10 MHz, 12.8 MHz and 7.68 MHz --- > 40 kHz

    2, Set PDF1 = 40 kHz

    3, Select Feedback_MUX from CLKout0 7.68 MHz

    4, Increase CP1 to 1.6 mA to against VCXO leakage current under low frequency PDF condition

    5, Set PLL1_WND_SIZE to 40 ns in "User Controls" sheet to against VCXO leakage current

    If there is no necessary to use 0-delay, then we can use 200 kHz PDF1 for 10 MHz and 12.8 MHz references, which can defense VCXO leakage current better than lower 80kHz or 40 kHz.

    For the topic about VCXO current leakage, refer to my notes, attached.

    4370.VCXO Leakage Current and PLL Lock v1.0.pdf