This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2491: LMX2491 Evaluation board

Part Number: LMX2491
Other Parts Discussed in Thread: LMX2492, LMX2492EVM,

Hello Team,

I do see that the LMX2491 evaluation board is not available for purchase. Only the LMX2492 is available.

What are the options to test the LMX2491?

If the LMX2492 would be the only options, how can I compare the results?

Would the performance up to 6GHz the same?

Thanks,

SunSet