This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE913: CDCE913 support in Linux version 4.14.0

Part Number: CDCE913
Other Parts Discussed in Thread: CDCE925, CDCEL913, CDCEL925

Hi all,

We are using Zynq-7000 in our custom board and Linux version 4.14.0.

We are using CDCE913 clock synthesizer in our custom board and have to configure for 100Mhz.

Linux version 4.14.0 has driver for cdce925 and it is mentioned that this driver support CDCE913 also.

I have added the entry for CDCE913 in my dts file as below:

cdce925@65 {
#clock-cells = <1>;
clocks = <&xtal>;
compatible = "ti,cdce913";
reg = <0x65>;
ti,input-clock-type = "xtal";
clock-names = "ref";
clock-output-names = "pll", "pll-switched";
PLL1 {
spread-spectrum = <4>;
clock-frequency = <100000000>, <100000000>, <100000000>;
spread-spectrum-center;
};

xtal: xtal {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <25000000>;
clock-output-names = "xtal";
};
};

I have added the prints in probe to find out that driver is getting called at the booting , and I  can see that probe function is getting called.

But when I probe the output clock I am getting 25Mhz which is the default clock frequency.

I doubt that CDCE913 is not getting configured properly. 

Whether I am missing something in the dts entry ?

Any other configuration is required for CDCE925 driver to work with CDCE913 chip?

Please suggest.

Regards,

Mahima Shanbag

  • Hi Mahima,

    Not sure I understand the question. CDCE913 uses standard I2C interface and doesn't require any driver. What driver are you referring to?

    Regards,

    Hao

  • Hi Hao,

    I think you didnt understand the question.

     CDCE913 chip is connected to Zynq-7000 PS through I2C interface.

    Before I was using Linux version 4.0.0 in which clk-cdce913.c driver was there, I am able to configure the  CDCE913 chip successfully and able to get 100Mhz output.

    I have attached the clk-cdce913.c for your reference.

    #include <linux/clk-provider.h>
    #include <linux/delay.h>
    #include <linux/gcd.h>
    #include <linux/i2c.h>
    #include <linux/lcm.h>
    #include <linux/module.h>
    #include <linux/regmap.h>
    #include <linux/slab.h>
    
    #define CDCE913_NUM_OUTPUTS	3
    
    /* CDCE913 registers */
    #define CDCE913_GENERIC_CFG_0	0x80
    #define CDCE913_GENERIC_CFG_1	0x81
    #define CDCE913_GENERIC_CFG_2	0x82
    #define CDCE913_GENERIC_CFG_3	0x83
    #define CDCE913_GENERIC_CFG_4	0x84
    #define CDCE913_GENERIC_CFG_5	0x85
    #define CDCE913_GENERIC_CFG_6	0x86
    
    #define CDCE913_PLL_CFG_0	0x90
    #define CDCE913_PLL_CFG_1	0x91
    #define CDCE913_PLL_CFG_2	0x92
    #define CDCE913_PLL_CFG_3	0x93
    #define CDCE913_PLL_CFG_4	0x94
    #define CDCE913_PLL_CFG_5	0x95
    #define CDCE913_PLL_CFG_6	0x96
    #define CDCE913_PLL_CFG_7	0x97
    #define CDCE913_PLL_CFG_8	0x98
    #define CDCE913_PLL_CFG_9	0x99
    #define CDCE913_PLL_CFG_10	0x9a
    #define CDCE913_PLL_CFG_11	0x9b
    #define CDCE913_PLL_CFG_12	0x9c
    #define CDCE913_PLL_CFG_13	0x9d
    #define CDCE913_PLL_CFG_14	0x9e
    #define CDCE913_PLL_CFG_15	0x9f
    
    /* bitfields */
    #define GENERIC_CFG0_DEVID_SHIFT	7
    #define GENERIC_CFG0_DEVID_MASK		(1 << GENERIC_CFG0_DEVID_SHIFT)
    #define GENERIC_CFG0_REVID_SHIFT	4
    #define GENERIC_CFG0_REVID_MASK		(7 << GENERIC_CFG0_REVID_SHIFT)
    #define GENERIC_CFG0_VENDORID_SHIFT	0
    #define GENERIC_CFG0_VENDORID_MASK	(0xf << GENERIC_CFG0_VENDORID_SHIFT)
    
    #define PLLCFG_N_UPPER_SHIFT	4
    #define PLLCFG_N_LOWER_SHIFT	4
    #define PLLCFG_N_LOWER_MASK	(0xf << PLLCFG_N_LOWER_SHIFT)
    #define PLLCFG_N_MAX		4095
    #define PLLCFG_N_MIN		1
    
    #define PLLCFG_M_MAX		511
    #define PLLCFG_M_MIN		1
    
    #define PLLCFG_R_UPPER_MASK	0xf
    #define PLLCFG_R_LOWER_SHIFT	3
    #define PLLCFG_R_LOWER_MASK	(0x1f << PLLCFG_R_LOWER_SHIFT)
    
    #define PLLCFG_Q_UPPER_MASK	7
    #define PLLCFG_Q_LOWER_SHIFT	5
    #define PLLCFG_Q_LOWER_MASK	(7 << PLLCFG_Q_LOWER_SHIFT)
    
    #define PLLCFG_P_SHIFT		2
    #define PLLCFG_P_MASK		(7 << PLLCFG_P_SHIFT)
    
    #define PDIV1_UPPER_MASK	3
    
    #define XTAL_LOAD_CAP_SHIFT	3
    #define XTAL_LOAD_CAP_MASK	(0x1f << XTAL_LOAD_CAP_SHIFT)
    
    #define CLK_IN_TYPE_SHIFT	2
    #define CLK_IN_TYPE_MASK	(3 << CLK_IN_TYPE_SHIFT)
    
    #define F_VCO_MIN		80000000
    #define F_VCO_MAX		230000000
    
    /**
     * struct clk_cdce913:
     * @regmap:	Device's regmap
     * @i2c_client:	I2C client pointer
     * @clk_out:	Handles to output clocks
     * @clk_data:	Onecell data struct
     * @s0:		State of config pin S0
     * @fsbit:	State of FS bit
     */
    struct clk_cdce913 {
    	struct regmap		*regmap;
    	struct i2c_client	*i2c_client;
    	struct clk		*clk_out[CDCE913_NUM_OUTPUTS];
    	struct clk_onecell_data	clk_data;
    	int			s0;
    	int			fsbit;
    };
    
    /**
     * struct clk_cdce913_pll:
     * @hw:		Clock handle
     * @frequency:	PLL frequency
     * @cdce913:	Pointer to driver struct
     */
    struct clk_cdce913_pll {
    	struct clk_hw		hw;
    	unsigned long		frequency;
    	struct clk_cdce913	*cdce913;
    };
    #define to_clk_cdce913_pll(_hw)	container_of(_hw, struct clk_cdce913_pll, hw)
    
    /* CDCE913 PLL */
    static int cdce913_read_pll_cfg(struct clk_cdce913 *cdce913, unsigned int *N,
    		unsigned int *R, unsigned int *Q, unsigned int *P)
    {
    	int err, i;
    	unsigned int addr;
    	unsigned int regs[4];
    
    	if (cdce913->fsbit)
    		addr = CDCE913_PLL_CFG_12;
    	else
    		addr = CDCE913_PLL_CFG_8;
    
    	for (i = 0; i < ARRAY_SIZE(regs); i++) {
    		err = regmap_read(cdce913->regmap, addr + i, &regs[i]);
    		if (err)
    			return err;
    	}
    
    	*N = (regs[0] << 4) |
    		((regs[1] & PLLCFG_N_LOWER_MASK) >> PLLCFG_N_LOWER_SHIFT);
    	*R = ((regs[1] & PLLCFG_R_UPPER_MASK) << 5) |
    		((regs[2] & PLLCFG_R_LOWER_MASK) >> PLLCFG_R_LOWER_SHIFT);
    	*Q = ((regs[2] & PLLCFG_Q_UPPER_MASK) << 3) |
    		((regs[3] & PLLCFG_Q_LOWER_MASK) >> PLLCFG_Q_LOWER_SHIFT);
    	*P = (regs[3] & PLLCFG_P_MASK) >> PLLCFG_P_SHIFT;
    
    	/* TODO make dev_dbg */
    	dev_info(&cdce913->i2c_client->dev, "%s: N=%u, R=%u, Q=%u, P=%u\n",
    			__func__, *N, *R, *Q, *P);
    
    	return 0;
    }
    
    static unsigned long cdce913_pll_recalc_rate(struct clk_hw *hw,
    		unsigned long parent_rate)
    {
    	int err;
    	u64 rate;
    	unsigned int N, R, Q, P;
    	struct clk_cdce913_pll *pll = to_clk_cdce913_pll(hw);
    	struct clk_cdce913 *cdce913 = pll->cdce913;
    
    	err = cdce913_read_pll_cfg(cdce913, &N, &R, &Q, &P);
    	if (err)
    		return pll->frequency;
    
    	rate = (N * Q) * (u64)parent_rate;
    	rate = div_u64(rate, N * (1 << P) - R);
    
    	pll->frequency = rate;
    
    	return pll->frequency;
    }
    
    static int cdce913_pll_calc_divs(unsigned long rate, unsigned long parent_rate,
    		unsigned int *N, int *R, unsigned int *Q, int *P)
    {
    	unsigned int NN, M, div;
    
    	div = gcd(rate, parent_rate);
    
    	*N = rate / div;
    	M = parent_rate / div;
    
    	if (*N > PLLCFG_N_MAX) {
    		div = DIV_ROUND_UP(*N, PLLCFG_N_MAX);
    		*N /= div;
    		M /= div;
    	}
    
    	if (M > PLLCFG_M_MAX) {
    		div = DIV_ROUND_UP(M, PLLCFG_M_MAX);
    		*N /= div;
    		M /= div;
    	}
    
    	if (!*N)
    		*N = PLLCFG_N_MIN;
    	if (!M)
    		M = PLLCFG_M_MIN;
    
    	if (*N < M)
    		return -EINVAL;
    
    	*P = 4 - ilog2(*N / M);
    	if (*P < 0)
    		*P = 0;
    
    	if (*P > 7)
    		return -EINVAL;
    
    	NN = *N * (1 << *P);
    
    	*Q = NN / M;
    	if (*Q < 16 || *Q > 63)
    		return -EINVAL;
    
    	*R = NN - M * *Q;
    	if (*R < 0 || *R > 511)
    		return -EINVAL;
    
    	return 0;
    }
    
    static long cdce913_pll_round_rate(struct clk_hw *hw, unsigned long rate,
    		unsigned long *parent_rate)
    {
    	u64 rrate;
    	int err, P, R;
    	unsigned int N, Q;
    	struct clk_cdce913_pll *pll = to_clk_cdce913_pll(hw);
    
    	if (rate > F_VCO_MAX)
    		rate = F_VCO_MAX;
    	if (rate < F_VCO_MIN)
    		rate = F_VCO_MIN;
    
    	err = cdce913_pll_calc_divs(rate, *parent_rate, &N, &R, &Q, &P);
    	if (err)
    		return pll->frequency;
    
    	rrate = (N * Q) * (u64)*parent_rate;
    	rrate = div_u64(rrate, N * (1 << P) - R);
    
    	return rrate;
    }
    
    static int cdce913_rate2range(unsigned long fvco)
    {
    	if (fvco < 125000000)
    		return 0;
    
    	if (fvco < 150000000)
    		return 1;
    
    	if (fvco < 175000000)
    		return 2;
    
    	return 3;
    }
    
    static int cdce913_write_pll_cfg(struct clk_cdce913 *cdce913, unsigned int N,
    		unsigned int R, unsigned int Q, unsigned int P,
    		unsigned int range)
    {
    	int err, i;
    	unsigned int addr;
    	unsigned int regs[4];
    
    	if (cdce913->fsbit)
    		addr = CDCE913_PLL_CFG_12;
    	else
    		addr = CDCE913_PLL_CFG_8;
    
    	regs[0] = N >> PLLCFG_N_UPPER_SHIFT;
    
    	regs[1] = (N << PLLCFG_N_LOWER_SHIFT) & PLLCFG_N_LOWER_MASK;
    	regs[1] |= R >> 5;
    
    	regs[2] = (R << PLLCFG_R_LOWER_SHIFT) & PLLCFG_R_LOWER_MASK;
    	regs[2] |= Q >> 3;
    
    	regs[3] = (Q << PLLCFG_Q_LOWER_SHIFT) & PLLCFG_Q_LOWER_MASK;
    	regs[3] |= P << PLLCFG_P_SHIFT;
    	regs[3] |= range;
    
    	/* TODO remove dbg stuff */
    	dev_info(&cdce913->i2c_client->dev, "%s: N=%u, R=%u, Q=%u, P=%u\n",
    			__func__, N, R, Q, P);
    
    	for (i = 0; i < ARRAY_SIZE(regs); i++) {
    		err = regmap_write(cdce913->regmap, addr + i, regs[i]);
    		if (err)
    			return err;
    	}
    
    	/* TODO remove dbg stuff */
    	cdce913_read_pll_cfg(cdce913, &N, &R, &Q, &P);
    
    	return err;
    }
    
    static int cdce913_pll_set_rate(struct clk_hw *hw, unsigned long rate,
    		unsigned long parent_rate)
    {
    	int err, P, R;
    	unsigned int N, Q;
    	struct clk_cdce913_pll *pll = to_clk_cdce913_pll(hw);
    	struct clk_cdce913 *cdce913 = pll->cdce913;
    
    	if (rate > F_VCO_MAX || rate < F_VCO_MIN)
    		return -EINVAL;
    
    	err = cdce913_pll_calc_divs(rate, parent_rate, &N, &R, &Q, &P);
    	if (err)
    		return err;
    
    	/* write to HW */
    	return cdce913_write_pll_cfg(cdce913, N, R, Q, P,
    			cdce913_rate2range(rate));
    }
    
    static struct clk_ops cdce913_pll_ops = {
    	.recalc_rate = cdce913_pll_recalc_rate,
    	.round_rate = cdce913_pll_round_rate,
    	.set_rate = cdce913_pll_set_rate,
    };
    
    static struct clk *clk_register_cdce913_pll(struct clk_cdce913 *cdce913,
    		const char *name, const char *parent)
    {
    	struct clk *clk;
    	const char *pll_name;
    	struct clk_init_data init;
    	struct clk_cdce913_pll *data;
    	const char *parents[] = {parent};
    
    	data = devm_kzalloc(&cdce913->i2c_client->dev, sizeof(*data),
    			GFP_KERNEL);
    	if (!data)
    		return ERR_PTR(-ENOMEM);
    
    	pll_name = kasprintf(GFP_KERNEL, "%s_pll", name);
    	if (!pll_name)
    		return ERR_PTR(-ENOMEM);
    
    	init.ops = &cdce913_pll_ops;
    	init.name = pll_name;
    	init.num_parents = 1;
    	init.parent_names = parents;
    	data->hw.init = &init;
    	data->cdce913 = cdce913;
    
    	clk = devm_clk_register(&cdce913->i2c_client->dev, &data->hw);
    
    	kfree(pll_name);
    
    	return clk;
    }
    
    /* PDIV1 accessors */
    static unsigned int pdiv1_get_div(struct clk_i2c_divider *divider)
    {
    	int err, i;
    	unsigned int regs[2];
    	unsigned int div;
    
    	for (i = 0; i < ARRAY_SIZE(regs); i++) {
    		err = regmap_read(divider->regmap, divider->reg + i, &regs[i]);
    		if (err)
    			break;
    	}
    	if (err) {
    		pr_err("%s: reading from device failed\n", __func__);
    		return 1;
    	}
    
    	div = (regs[0] & PDIV1_UPPER_MASK) << 8;
    	div |= regs[1];
    
    	return div;
    }
    
    static int pdiv1_set_div(unsigned int div, struct clk_i2c_divider *divider)
    {
    	int err, i;
    	unsigned int regs[2];
    
    	for (i = 0; i < ARRAY_SIZE(regs); i++) {
    		err = regmap_read(divider->regmap, divider->reg + i, &regs[i]);
    		if (err)
    			return err;
    	}
    
    	regs[1] = div & 0xff;
    
    	regs[0] &= ~PDIV1_UPPER_MASK;
    	div >>= 8;
    	div &= PDIV1_UPPER_MASK;
    	regs[0] |= div;
    
    	for (i = 0; i < ARRAY_SIZE(regs); i++) {
    		err = regmap_write(divider->regmap, divider->reg + i, regs[i]);
    		if (err)
    			return err;
    	}
    
    	return 0;
    }
    
    /* regmap functions */
    static bool cdce913_regmap_is_volatile(struct device *dev, unsigned int reg)
    {
    	switch (reg) {
    	case CDCE913_GENERIC_CFG_1:
    		return true;
    	default:
    		return false;
    	}
    }
    
    static bool cdce913_regmap_is_writeable(struct device *dev, unsigned int reg)
    {
    	switch (reg) {
    	case CDCE913_GENERIC_CFG_1 ... CDCE913_GENERIC_CFG_6:
    		return true;
    	case CDCE913_PLL_CFG_0 ... CDCE913_PLL_CFG_15:
    		return true;
    	default:
    		return false;
    	}
    }
    
    static struct regmap_config cdce913_regmap_config = {
    	.reg_bits = 8,
    	.val_bits = 8,
    	.cache_type = REGCACHE_RBTREE,
    	.max_register = CDCE913_PLL_CFG_15,
    	.writeable_reg = cdce913_regmap_is_writeable,
    	.volatile_reg = cdce913_regmap_is_volatile,
    };
    
    /**
     * cdce913_get_part_id() - Read part identification
     * @cdce913:	Driver data structure
     * @dev:	Part ID (output)
     * @rev:	Part revision (output)
     * @ven:	Vendor ID (output)
     * Returns 0 on success, or passes on regmap_read() error.
     */
    static int cdce913_get_part_id(struct clk_cdce913 *cdce913, unsigned int *dev,
    		unsigned int *rev, unsigned int *ven)
    {
    	int err;
    	unsigned int reg;
    
    	err = regmap_read(cdce913->regmap, CDCE913_GENERIC_CFG_0, &reg);
    	if (err)
    		return err;
    
    	*rev = (reg & GENERIC_CFG0_REVID_MASK) >> GENERIC_CFG0_DEVID_SHIFT;
    	*ven = (reg & GENERIC_CFG0_VENDORID_MASK) >> GENERIC_CFG0_VENDORID_SHIFT;
    	*dev = (reg & GENERIC_CFG0_DEVID_MASK) >> GENERIC_CFG0_DEVID_SHIFT;
    
    	return 0;
    }
    
    /**
     * cdce913_set_clk_in_type() - Set input clock type
     * @cdce913:		Driver data structure
     * @clk_in_type:	String describing input clock type
     *
     * Set the input clock type according to the provided DT property. Valid types
     * are 'xtal', 'VCXO', 'LVCMOS'.
     */
    static void cdce913_set_clk_in_type(struct clk_cdce913 *cdce913,
    		const char *clk_in_type)
    {
    	int err;
    	unsigned int type, reg;
    	/*
    	 * Valid types are xtal, VCXO, LVCMOS, let's do a lazy compare of the
    	 * first letter only and save us all the strcmp overhead
    	 */
    	switch (clk_in_type[0]) {
    	case 'V':
    		type = 1;
    		break;
    	case 'L':
    		type = 2;
    		break;
    	default:
    		type = 0;
    		break;
    	}
    
    	err = regmap_read(cdce913->regmap, CDCE913_GENERIC_CFG_1, &reg);
    	if (err) {
    		dev_err(&cdce913->i2c_client->dev, "read from device failed\n");
    		return;
    	}
    
    	reg &= ~CLK_IN_TYPE_MASK;
    	reg |= type << CLK_IN_TYPE_SHIFT;
    
    	err = regmap_write(cdce913->regmap, CDCE913_GENERIC_CFG_1, reg);
    	if (err) {
    		dev_err(&cdce913->i2c_client->dev, "write to device failed\n");
    		return;
    	}
    }
    
    static void cdce913_init_frequencies(struct device_node *np,
    		struct clk_cdce913 *data, struct clk *pll)
    {
    	int err, i;
    	u32 fout[3];
    	unsigned long fvco;
    	struct device *dev = &data->i2c_client->dev;
    
    	err = of_property_read_u32_array(np, "clock-frequency", fout,
    			ARRAY_SIZE(fout));
    	if (err)
    		return;
    
    	for (i = 0; i < ARRAY_SIZE(fout); i++) {
    		if (fout[i] > F_VCO_MAX) {
    			dev_warn(dev, "requested output frequency '%u' exceeds maximum (%u)\n",
    					fout[i], F_VCO_MAX);
    			fout[i] = F_VCO_MAX;
    		}
    	}
    
    	fvco = lcm(fout[0] / 1000000, fout[1] / 1000000);
    	fvco = lcm(fvco, fout[2] / 1000000);
    	fvco *= 1000000;
    
    	if (fvco > F_VCO_MAX) {
    		dev_warn(dev, "requested VCO frequency '%lu' exceeds maximum (%u)\n",
    				fvco, F_VCO_MAX);
    		fvco = F_VCO_MAX;
    	}
    
    	if (fvco < F_VCO_MIN) {
    		dev_warn(dev, "requested VCO frequency '%lu' below minimum (%u)\n",
    				fvco, F_VCO_MIN);
    		fvco = F_VCO_MIN;
    	}
    
    	err = clk_set_rate(pll, fvco);
    	if (err)
    		return;
    
    	/* TODO dev_dbg */
    	dev_info(dev, "VCO frequency: %lu Hz\n", clk_get_rate(pll));
    
    	for (i = 0; i < ARRAY_SIZE(fout); i++) {
    		if (fout[i])
    			clk_set_rate(data->clk_out[i], fout[i]);
    	}
    }
    
    static int cdce913_probe(struct i2c_client *client,
    		const struct i2c_device_id *id)
    {
    	int err;
    	unsigned int part, revision, vendor, cap;
    	struct clk_cdce913 *data;
    	struct clk *pll, *pll_mux, *y1_mux, *y2_mux, *y3_mux;
    	struct clk *pdiv1, *pdiv2, *pdiv3;
    	const char *pname, *pll_mux_name, *clk_in_type;
    	const char *y1_mux_name, *y2_mux_name, *y3_mux_name;
    	const char *pdiv1_name, *pdiv2_name, *pdiv3_name;
    	const char *pll_mux_parents[2];
    	const char *y1_mux_parents[2], *y2_mux_parents[2], *y3_mux_parents[3];
    	struct device_node *np = client->dev.of_node;
    
    	data = devm_kzalloc(&client->dev, sizeof(*data), GFP_KERNEL);
    	if (!data)
    		return -ENOMEM;
    
    	data->i2c_client = client;
    
    	data->regmap = devm_regmap_init_i2c(client, &cdce913_regmap_config);
    	if (IS_ERR(data->regmap)) {
    		dev_err(&client->dev, "failed to allocate register map\n");
    		return PTR_ERR(data->regmap);
    	}
    
    	err = of_property_read_u32(np, "ti,s0", &data->s0);
    	if (err) {
    		dev_warn(&client->dev, "S0 not specified, assuming 1\n");
    		data->s0 = 1;
    	}
    
    	err = regmap_read(data->regmap, CDCE913_PLL_CFG_3, &data->fsbit);
    	if (err) {
    		dev_warn(&client->dev, "unable to read from device\n");
    		return err;
    	}
    	data->fsbit = !!(data->fsbit & (1 << data->s0));
    
    	i2c_set_clientdata(client, data);
    
    	err = cdce913_get_part_id(data, &part, &revision, &vendor);
    	if (err)
    		return err;
    
    	pname = of_clk_get_parent_name(np, 0);
    	if (!pname) {
    		dev_err(&client->dev, "no input clock specified\n");
    		return -ENODEV;
    	}
    
    	/* PLL */
    	pll = clk_register_cdce913_pll(data, np->name, pname);
    	if (IS_ERR(pll)) {
    		dev_err(&client->dev, "clock registration failed\n");
    		return PTR_ERR(pll);
    	}
    
    	/* PLL mux */
    	pll_mux_name = kasprintf(GFP_KERNEL, "%s_pll_mux", np->name);
    	if (!pll_mux_name)
    		return -ENOMEM;
    
    	pll_mux_parents[0] = __clk_get_name(pll);
    	pll_mux_parents[1] = pname;
    	pll_mux = clk_i2c_register_mux(&client->dev, pll_mux_name,
    			pll_mux_parents, 2, CLK_SET_RATE_PARENT, data->regmap,
    			CDCE913_PLL_CFG_4, 7, 1, 0);
    	if (IS_ERR(pll_mux)) {
    		dev_err(&client->dev, "clock registration failed\n");
    		err = PTR_ERR(pll_mux);
    		goto err_pll_mux;
    	}
    
    	/* use PLL */
    	err = clk_set_parent(pll_mux, pll);
    	if (err)
    		dev_warn(&client->dev, "PLL in bypass\n");
    
    	/* Y1 mux */
    	y1_mux_name = kasprintf(GFP_KERNEL, "%s_y1_mux", np->name);
    	if (!y1_mux_name) {
    		err = -ENOMEM;
    		goto err_pll_mux;
    	}
    
    	y1_mux_parents[0] = pname;
    	y1_mux_parents[1] = pll_mux_name;
    	y1_mux = clk_i2c_register_mux(&client->dev, y1_mux_name,
    			y1_mux_parents, 2,
    			CLK_SET_RATE_PARENT | CLK_SET_RATE_NO_REPARENT,
    			data->regmap, CDCE913_GENERIC_CFG_2, 7, 1, 0);
    	if (IS_ERR(y1_mux)) {
    		dev_err(&client->dev, "clock registration failed\n");
    		err = PTR_ERR(y1_mux);
    		goto err_y1_mux;
    	}
    
    	/* pdiv1 */
    	pdiv1_name = kasprintf(GFP_KERNEL, "%s_pdiv1", np->name);
    	if (!pdiv1_name) {
    		err = -ENOMEM;
    		goto err_y1_mux;
    	}
    
    	pdiv1 = clk_i2c_register_divider(&client->dev, pdiv1_name, y1_mux_name,
    			CLK_SET_RATE_PARENT, data->regmap, CDCE913_GENERIC_CFG_2, 0, 10,
    			CLK_DIVIDER_ONE_BASED, pdiv1_get_div, pdiv1_set_div);
    	if (IS_ERR(pdiv1)) {
    		dev_err(&client->dev, "clock registration failed\n");
    		err = PTR_ERR(pdiv1);
    		goto err_pdiv1;
    	}
    
    	/* pdiv2 */
    	pdiv2_name = kasprintf(GFP_KERNEL, "%s_pdiv2", np->name);
    	if (!pdiv2_name) {
    		err = -ENOMEM;
    		goto err_pdiv1;
    	}
    
    	pdiv2 = clk_i2c_register_divider(&client->dev, pdiv2_name,
    			pll_mux_name, CLK_SET_RATE_PARENT, data->regmap,
    			CDCE913_PLL_CFG_6, 0, 7, CLK_DIVIDER_ONE_BASED, NULL,
    			NULL);
    	if (IS_ERR(pdiv2)) {
    		dev_err(&client->dev, "clock registration failed\n");
    		err = PTR_ERR(pdiv2);
    		goto err_pdiv2;
    	}
    
    	/* pdiv3 */
    	pdiv3_name = kasprintf(GFP_KERNEL, "%s_pdiv3", np->name);
    	if (!pdiv3_name) {
    		err = -ENOMEM;
    		goto err_pdiv2;
    	}
    
    	pdiv3 = clk_i2c_register_divider(&client->dev, pdiv3_name,
    			pll_mux_name, CLK_SET_RATE_PARENT, data->regmap,
    			CDCE913_PLL_CFG_7, 0, 7, CLK_DIVIDER_ONE_BASED, NULL,
    			NULL);
    	if (IS_ERR(pdiv3)) {
    		dev_err(&client->dev, "clock registration failed\n");
    		err = PTR_ERR(pdiv3);
    		goto err_pdiv3;
    	}
    
    	/* Y2 mux */
    	y2_mux_name = kasprintf(GFP_KERNEL, "%s_y2_mux", np->name);
    	if (!y2_mux_name) {
    		err = -ENOMEM;
    		goto err_pdiv3;
    	}
    
    	y2_mux_parents[0] = pdiv1_name;
    	y2_mux_parents[1] = pdiv2_name;
    	y2_mux = clk_i2c_register_mux(&client->dev, y2_mux_name,
    			y2_mux_parents, 2,
    			CLK_SET_RATE_PARENT | CLK_SET_RATE_NO_REPARENT,
    			data->regmap, CDCE913_PLL_CFG_4, 6, 1, 0);
    	if (IS_ERR(y2_mux)) {
    		dev_err(&client->dev, "clock registration failed\n");
    		err = PTR_ERR(y2_mux);
    		goto err_y2_mux;
    	}
    
    	/* Y3 mux */
    	y3_mux_name = kasprintf(GFP_KERNEL, "%s_y3_mux", np->name);
    	if (!y3_mux_name) {
    		err = -ENOMEM;
    		goto err_y2_mux;
    	}
    
    	y3_mux_parents[0] = pdiv1_name;
    	y3_mux_parents[1] = pdiv2_name;
    	y3_mux_parents[2] = pdiv3_name;
    	y3_mux = clk_i2c_register_mux(&client->dev, y3_mux_name,
    			y3_mux_parents, 3,
    			CLK_SET_RATE_PARENT | CLK_SET_RATE_NO_REPARENT,
    			data->regmap, CDCE913_PLL_CFG_4, 4, 2, 0);
    	if (IS_ERR(y3_mux)) {
    		dev_err(&client->dev, "clock registration failed\n");
    		err = PTR_ERR(y3_mux);
    		goto err_y3_mux;
    	}
    
    	err = of_property_read_u32(np, "ti,crystal-load-capacity", &cap);
    	if (!err) {
    		if (cap > 20)
    			cap = 20;
    		cap <<= XTAL_LOAD_CAP_SHIFT;
    		err = regmap_write(data->regmap, CDCE913_GENERIC_CFG_5, cap);
    		if (err)
    			dev_warn(&client->dev, "unable to write to device\n");
    	}
    
    	err = of_property_read_string(np, "ti,input-clock-type", &clk_in_type);
    	if (!err)
    		cdce913_set_clk_in_type(data, clk_in_type);
    
    err_y3_mux:
    	kfree(y3_mux_name);
    err_y2_mux:
    	kfree(y2_mux_name);
    err_pdiv3:
    	kfree(pdiv3_name);
    err_pdiv2:
    	kfree(pdiv2_name);
    err_pdiv1:
    	kfree(pdiv1_name);
    err_y1_mux:
    	kfree(y1_mux_name);
    err_pll_mux:
    	kfree(pll_mux_name);
    
    	if (err)
    		return err;
    
    	data->clk_out[0] = pdiv1;
    	data->clk_out[1] = y2_mux;
    	data->clk_out[2] = y3_mux;
    
    	data->clk_data.clks = data->clk_out;
    	data->clk_data.clk_num = ARRAY_SIZE(data->clk_out);
    	err = of_clk_add_provider(np, of_clk_src_onecell_get, &data->clk_data);
    	if (err)
    		goto err_clk_provider;
    
    	cdce913_init_frequencies(np, data, pll);
    
    	dev_info(&client->dev, "%s %u/%u: current frequencies: %lu, %lu, %lu\n",
    			part ? "CDCE913" : "CDCEL913", vendor, revision,
    			clk_get_rate(data->clk_out[0]),
    			clk_get_rate(data->clk_out[1]),
    			clk_get_rate(data->clk_out[2]));
    
    err_clk_provider:
    	return err;
    }
    
    static int cdce913_remove(struct i2c_client *client)
    {
    	of_clk_del_provider(client->dev.of_node);
    	return 0;
    }
    
    static const struct i2c_device_id cdce913_id[] = {
    	{ "cdce913" },
    	{ "cdcel913" },
    	{ }
    };
    MODULE_DEVICE_TABLE(i2c, cdce_id);
    
    static const struct of_device_id clk_cdce913_of_match[] = {
    	{ .compatible = "ti,cdce913" },
    	{ .compatible = "ti,cdcel913" },
    	{ },
    };
    MODULE_DEVICE_TABLE(of, clk_cdce913_of_match);
    
    static struct i2c_driver cdce913_driver = {
    	.driver = {
    		.name = "cdce913",
    		.of_match_table = of_match_ptr(clk_cdce913_of_match),
    	},
    	.probe		= cdce913_probe,
    	.remove		= cdce913_remove,
    	.id_table	= cdce913_id,
    };
    module_i2c_driver(cdce913_driver);
    
    MODULE_AUTHOR("Soeren Brinkmann <soren.brinkmann@xilinx.com");
    MODULE_DESCRIPTION("CDCE913 driver");
    MODULE_LICENSE("GPL");
    

    Now I have upgraded the Linux version to  4.14.0 and it has clk-cdce925.c driver.

    Here I am attaching clk-cdce925.c driver.

    /*
     * Driver for TI Multi PLL CDCE913/925/937/949 clock synthesizer
     *
     * This driver always connects the Y1 to the input clock, Y2/Y3 to PLL1,
     * Y4/Y5 to PLL2, and so on. PLL frequency is set on a first-come-first-serve
     * basis. Clients can directly request any frequency that the chip can
     * deliver using the standard clk framework. In addition, the device can
     * be configured and activated via the devicetree.
     *
     * Copyright (C) 2014, Topic Embedded Products
     * Licenced under GPL
     */
    #include <linux/clk.h>
    #include <linux/clk-provider.h>
    #include <linux/delay.h>
    #include <linux/module.h>
    #include <linux/i2c.h>
    #include <linux/regmap.h>
    #include <linux/slab.h>
    #include <linux/gcd.h>
    
    /* Each chip has different number of PLLs and outputs, for example:
     * The CECE925 has 2 PLLs which can be routed through dividers to 5 outputs.
     * Model this as 2 PLL clocks which are parents to the outputs.
     */
    
    enum {
    	CDCE913,
    	CDCE925,
    	CDCE937,
    	CDCE949,
    };
    
    struct clk_cdce925_chip_info {
    	int num_plls;
    	int num_outputs;
    };
    
    static const struct clk_cdce925_chip_info clk_cdce925_chip_info_tbl[] = {
    	[CDCE913] = { .num_plls = 1, .num_outputs = 3 },
    	[CDCE925] = { .num_plls = 2, .num_outputs = 5 },
    	[CDCE937] = { .num_plls = 3, .num_outputs = 7 },
    	[CDCE949] = { .num_plls = 4, .num_outputs = 9 },
    };
    
    #define MAX_NUMBER_OF_PLLS	4
    #define MAX_NUMBER_OF_OUTPUTS	9
    
    #define CDCE925_REG_GLOBAL1	0x81
    #define CDCE925_REG_Y1SPIPDIVH	0x82
    #define CDCE925_REG_PDIVL	0x83
    #define CDCE925_REG_XCSEL	0x85
    /* PLL parameters start at 0x10, steps of 0x10 */
    #define CDCE925_OFFSET_PLL	0x90
    /* Add CDCE925_OFFSET_PLL * (pll) to these registers before sending */
    #define CDCE925_PLL_MUX_OUTPUTS	0x94
    #define CDCE925_PLL_MULDIV	0x98
    
    #define CDCE925_PLL_FREQUENCY_MIN	 80000000ul
    #define CDCE925_PLL_FREQUENCY_MAX	230000000ul
    struct clk_cdce925_chip;
    
    struct clk_cdce925_output {
    	struct clk_hw hw;
    	struct clk_cdce925_chip *chip;
    	u8 index;
    	u16 pdiv; /* 1..127 for Y2-Y9; 1..1023 for Y1 */
    };
    #define to_clk_cdce925_output(_hw) \
    	container_of(_hw, struct clk_cdce925_output, hw)
    
    struct clk_cdce925_pll {
    	struct clk_hw hw;
    	struct clk_cdce925_chip *chip;
    	u8 index;
    	u16 m;   /* 1..511 */
    	u16 n;   /* 1..4095 */
    };
    #define to_clk_cdce925_pll(_hw)	container_of(_hw, struct clk_cdce925_pll, hw)
    
    struct clk_cdce925_chip {
    	struct regmap *regmap;
    	struct i2c_client *i2c_client;
    	const struct clk_cdce925_chip_info *chip_info;
    	struct clk_cdce925_pll pll[MAX_NUMBER_OF_PLLS];
    	struct clk_cdce925_output clk[MAX_NUMBER_OF_OUTPUTS];
    };
    
    /* ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** */
    
    static unsigned long cdce925_pll_calculate_rate(unsigned long parent_rate,
    	u16 n, u16 m)
    {
    	if ((!m || !n) || (m == n))
    		return parent_rate; /* In bypass mode runs at same frequency */
    	return mult_frac(parent_rate, (unsigned long)n, (unsigned long)m);
    }
    
    static unsigned long cdce925_pll_recalc_rate(struct clk_hw *hw,
    		unsigned long parent_rate)
    {
    	/* Output frequency of PLL is Fout = (Fin/Pdiv)*(N/M) */
    	struct clk_cdce925_pll *data = to_clk_cdce925_pll(hw);
    
    	return cdce925_pll_calculate_rate(parent_rate, data->n, data->m);
    }
    
    static void cdce925_pll_find_rate(unsigned long rate,
    		unsigned long parent_rate, u16 *n, u16 *m)
    {
    	unsigned long un;
    	unsigned long um;
    	unsigned long g;
    
    	if (rate <= parent_rate) {
    		/* Can always deliver parent_rate in bypass mode */
    		rate = parent_rate;
    		*n = 0;
    		*m = 0;
    	} else {
    		/* In PLL mode, need to apply min/max range */
    		if (rate < CDCE925_PLL_FREQUENCY_MIN)
    			rate = CDCE925_PLL_FREQUENCY_MIN;
    		else if (rate > CDCE925_PLL_FREQUENCY_MAX)
    			rate = CDCE925_PLL_FREQUENCY_MAX;
    
    		g = gcd(rate, parent_rate);
    		um = parent_rate / g;
    		un = rate / g;
    		/* When outside hw range, reduce to fit (rounding errors) */
    		while ((un > 4095) || (um > 511)) {
    			un >>= 1;
    			um >>= 1;
    		}
    		if (un == 0)
    			un = 1;
    		if (um == 0)
    			um = 1;
    
    		*n = un;
    		*m = um;
    	}
    }
    
    static long cdce925_pll_round_rate(struct clk_hw *hw, unsigned long rate,
    		unsigned long *parent_rate)
    {
    	u16 n, m;
    
    	cdce925_pll_find_rate(rate, *parent_rate, &n, &m);
    	return (long)cdce925_pll_calculate_rate(*parent_rate, n, m);
    }
    
    static int cdce925_pll_set_rate(struct clk_hw *hw, unsigned long rate,
    		unsigned long parent_rate)
    {
    	struct clk_cdce925_pll *data = to_clk_cdce925_pll(hw);
    
    	if (!rate || (rate == parent_rate)) {
    		data->m = 0; /* Bypass mode */
    		data->n = 0;
    		return 0;
    	}
    
    	if ((rate < CDCE925_PLL_FREQUENCY_MIN) ||
    		(rate > CDCE925_PLL_FREQUENCY_MAX)) {
    		pr_debug("%s: rate %lu outside PLL range.\n", __func__, rate);
    		return -EINVAL;
    	}
    
    	if (rate < parent_rate) {
    		pr_debug("%s: rate %lu less than parent rate %lu.\n", __func__,
    			rate, parent_rate);
    		return -EINVAL;
    	}
    
    	cdce925_pll_find_rate(rate, parent_rate, &data->n, &data->m);
    	return 0;
    }
    
    
    /* calculate p = max(0, 4 - int(log2 (n/m))) */
    static u8 cdce925_pll_calc_p(u16 n, u16 m)
    {
    	u8 p;
    	u16 r = n / m;
    
    	if (r >= 16)
    		return 0;
    	p = 4;
    	while (r > 1) {
    		r >>= 1;
    		--p;
    	}
    	return p;
    }
    /* Returns VCO range bits for VCO1_0_RANGE */
    static u8 cdce925_pll_calc_range_bits(struct clk_hw *hw, u16 n, u16 m)
    {
    	struct clk *parent = clk_get_parent(hw->clk);
    	unsigned long rate = clk_get_rate(parent);
    
    	rate = mult_frac(rate, (unsigned long)n, (unsigned long)m);
    	if (rate >= 175000000)
    		return 0x3;
    	if (rate >= 150000000)
    		return 0x02;
    	if (rate >= 125000000)
    		return 0x01;
    	return 0x00;
    }
    
    /* I2C clock, hence everything must happen in (un)prepare because this
     * may sleep */
    static int cdce925_pll_prepare(struct clk_hw *hw)
    {
    	struct clk_cdce925_pll *data = to_clk_cdce925_pll(hw);
    	u16 n = data->n;
    	u16 m = data->m;
    	u16 r;
    	u8 q;
    	u8 p;
    	u16 nn;
    	u8 pll[4]; /* Bits are spread out over 4 byte registers */
    	u8 reg_ofs = data->index * CDCE925_OFFSET_PLL;
    	unsigned i;
    
    	if ((!m || !n) || (m == n)) {
    		/* Set PLL mux to bypass mode, leave the rest as is */
    		regmap_update_bits(data->chip->regmap,
    			reg_ofs + CDCE925_PLL_MUX_OUTPUTS, 0x80, 0x80);
    	} else {
    		/* According to data sheet: */
    		/* p = max(0, 4 - int(log2 (n/m))) */
    		p = cdce925_pll_calc_p(n, m);
    		/* nn = n * 2^p */
    		nn = n * BIT(p);
    		/* q = int(nn/m) */
    		q = nn / m;
    		if ((q < 16) || (q > 63)) {
    			pr_debug("%s invalid q=%d\n", __func__, q);
    			return -EINVAL;
    		}
    		r = nn - (m*q);
    		if (r > 511) {
    			pr_debug("%s invalid r=%d\n", __func__, r);
    			return -EINVAL;
    		}
    		pr_debug("%s n=%d m=%d p=%d q=%d r=%d\n", __func__,
    			n, m, p, q, r);
    		/* encode into register bits */
    		pll[0] = n >> 4;
    		pll[1] = ((n & 0x0F) << 4) | ((r >> 5) & 0x0F);
    		pll[2] = ((r & 0x1F) << 3) | ((q >> 3) & 0x07);
    		pll[3] = ((q & 0x07) << 5) | (p << 2) |
    				cdce925_pll_calc_range_bits(hw, n, m);
    		/* Write to registers */
    		for (i = 0; i < ARRAY_SIZE(pll); ++i)
    			regmap_write(data->chip->regmap,
    				reg_ofs + CDCE925_PLL_MULDIV + i, pll[i]);
    		/* Enable PLL */
    		regmap_update_bits(data->chip->regmap,
    			reg_ofs + CDCE925_PLL_MUX_OUTPUTS, 0x80, 0x00);
    	}
    
    	return 0;
    }
    
    static void cdce925_pll_unprepare(struct clk_hw *hw)
    {
    	struct clk_cdce925_pll *data = to_clk_cdce925_pll(hw);
    	u8 reg_ofs = data->index * CDCE925_OFFSET_PLL;
    
    	regmap_update_bits(data->chip->regmap,
    			reg_ofs + CDCE925_PLL_MUX_OUTPUTS, 0x80, 0x80);
    }
    
    static const struct clk_ops cdce925_pll_ops = {
    	.prepare = cdce925_pll_prepare,
    	.unprepare = cdce925_pll_unprepare,
    	.recalc_rate = cdce925_pll_recalc_rate,
    	.round_rate = cdce925_pll_round_rate,
    	.set_rate = cdce925_pll_set_rate,
    };
    
    
    static void cdce925_clk_set_pdiv(struct clk_cdce925_output *data, u16 pdiv)
    {
    	switch (data->index) {
    	case 0:
    		regmap_update_bits(data->chip->regmap,
    			CDCE925_REG_Y1SPIPDIVH,
    			0x03, (pdiv >> 8) & 0x03);
    		regmap_write(data->chip->regmap, 0x03, pdiv & 0xFF);
    		break;
    	case 1:
    		regmap_update_bits(data->chip->regmap, 0x16, 0x7F, pdiv);
    		break;
    	case 2:
    		regmap_update_bits(data->chip->regmap, 0x17, 0x7F, pdiv);
    		break;
    	case 3:
    		regmap_update_bits(data->chip->regmap, 0x26, 0x7F, pdiv);
    		break;
    	case 4:
    		regmap_update_bits(data->chip->regmap, 0x27, 0x7F, pdiv);
    		break;
    	case 5:
    		regmap_update_bits(data->chip->regmap, 0x36, 0x7F, pdiv);
    		break;
    	case 6:
    		regmap_update_bits(data->chip->regmap, 0x37, 0x7F, pdiv);
    		break;
    	case 7:
    		regmap_update_bits(data->chip->regmap, 0x46, 0x7F, pdiv);
    		break;
    	case 8:
    		regmap_update_bits(data->chip->regmap, 0x47, 0x7F, pdiv);
    		break;
    	}
    }
    
    static void cdce925_clk_activate(struct clk_cdce925_output *data)
    {
    	switch (data->index) {
    	case 0:
    		regmap_update_bits(data->chip->regmap,
    			CDCE925_REG_Y1SPIPDIVH, 0x0c, 0x0c);
    		break;
    	case 1:
    	case 2:
    		regmap_update_bits(data->chip->regmap, 0x14, 0x03, 0x03);
    		break;
    	case 3:
    	case 4:
    		regmap_update_bits(data->chip->regmap, 0x24, 0x03, 0x03);
    		break;
    	case 5:
    	case 6:
    		regmap_update_bits(data->chip->regmap, 0x34, 0x03, 0x03);
    		break;
    	case 7:
    	case 8:
    		regmap_update_bits(data->chip->regmap, 0x44, 0x03, 0x03);
    		break;
    	}
    }
    
    static int cdce925_clk_prepare(struct clk_hw *hw)
    {
    	struct clk_cdce925_output *data = to_clk_cdce925_output(hw);
    
    	cdce925_clk_set_pdiv(data, data->pdiv);
    	cdce925_clk_activate(data);
    	return 0;
    }
    
    static void cdce925_clk_unprepare(struct clk_hw *hw)
    {
    	struct clk_cdce925_output *data = to_clk_cdce925_output(hw);
    
    	/* Disable clock by setting divider to "0" */
    	cdce925_clk_set_pdiv(data, 0);
    }
    
    static unsigned long cdce925_clk_recalc_rate(struct clk_hw *hw,
    		unsigned long parent_rate)
    {
    	struct clk_cdce925_output *data = to_clk_cdce925_output(hw);
    
    	if (data->pdiv)
    		return parent_rate / data->pdiv;
    	return 0;
    }
    
    static u16 cdce925_calc_divider(unsigned long rate,
    		unsigned long parent_rate)
    {
    	unsigned long divider;
    
    	if (!rate)
    		return 0;
    	if (rate >= parent_rate)
    		return 1;
    
    	divider = DIV_ROUND_CLOSEST(parent_rate, rate);
    	if (divider > 0x7F)
    		divider = 0x7F;
    
    	return (u16)divider;
    }
    
    static unsigned long cdce925_clk_best_parent_rate(
    	struct clk_hw *hw, unsigned long rate)
    {
    	struct clk *pll = clk_get_parent(hw->clk);
    	struct clk *root = clk_get_parent(pll);
    	unsigned long root_rate = clk_get_rate(root);
    	unsigned long best_rate_error = rate;
    	u16 pdiv_min;
    	u16 pdiv_max;
    	u16 pdiv_best;
    	u16 pdiv_now;
    
    	if (root_rate % rate == 0)
    		return root_rate; /* Don't need the PLL, use bypass */
    
    	pdiv_min = (u16)max(1ul, DIV_ROUND_UP(CDCE925_PLL_FREQUENCY_MIN, rate));
    	pdiv_max = (u16)min(127ul, CDCE925_PLL_FREQUENCY_MAX / rate);
    
    	if (pdiv_min > pdiv_max)
    		return 0; /* No can do? */
    
    	pdiv_best = pdiv_min;
    	for (pdiv_now = pdiv_min; pdiv_now < pdiv_max; ++pdiv_now) {
    		unsigned long target_rate = rate * pdiv_now;
    		long pll_rate = clk_round_rate(pll, target_rate);
    		unsigned long actual_rate;
    		unsigned long rate_error;
    
    		if (pll_rate <= 0)
    			continue;
    		actual_rate = pll_rate / pdiv_now;
    		rate_error = abs((long)actual_rate - (long)rate);
    		if (rate_error < best_rate_error) {
    			pdiv_best = pdiv_now;
    			best_rate_error = rate_error;
    		}
    		/* TODO: Consider PLL frequency based on smaller n/m values
    		 * and pick the better one if the error is equal */
    	}
    
    	return rate * pdiv_best;
    }
    
    static long cdce925_clk_round_rate(struct clk_hw *hw, unsigned long rate,
    		unsigned long *parent_rate)
    {
    	unsigned long l_parent_rate = *parent_rate;
    	u16 divider = cdce925_calc_divider(rate, l_parent_rate);
    
    	if (l_parent_rate / divider != rate) {
    		l_parent_rate = cdce925_clk_best_parent_rate(hw, rate);
    		divider = cdce925_calc_divider(rate, l_parent_rate);
    		*parent_rate = l_parent_rate;
    	}
    
    	if (divider)
    		return (long)(l_parent_rate / divider);
    	return 0;
    }
    
    static int cdce925_clk_set_rate(struct clk_hw *hw, unsigned long rate,
    		unsigned long parent_rate)
    {
    	struct clk_cdce925_output *data = to_clk_cdce925_output(hw);
    
    	data->pdiv = cdce925_calc_divider(rate, parent_rate);
    
    	return 0;
    }
    
    static const struct clk_ops cdce925_clk_ops = {
    	.prepare = cdce925_clk_prepare,
    	.unprepare = cdce925_clk_unprepare,
    	.recalc_rate = cdce925_clk_recalc_rate,
    	.round_rate = cdce925_clk_round_rate,
    	.set_rate = cdce925_clk_set_rate,
    };
    
    
    static u16 cdce925_y1_calc_divider(unsigned long rate,
    		unsigned long parent_rate)
    {
    	unsigned long divider;
    
    	if (!rate)
    		return 0;
    	if (rate >= parent_rate)
    		return 1;
    
    	divider = DIV_ROUND_CLOSEST(parent_rate, rate);
    	if (divider > 0x3FF) /* Y1 has 10-bit divider */
    		divider = 0x3FF;
    
    	return (u16)divider;
    }
    
    static long cdce925_clk_y1_round_rate(struct clk_hw *hw, unsigned long rate,
    		unsigned long *parent_rate)
    {
    	unsigned long l_parent_rate = *parent_rate;
    	u16 divider = cdce925_y1_calc_divider(rate, l_parent_rate);
    
    	if (divider)
    		return (long)(l_parent_rate / divider);
    	return 0;
    }
    
    static int cdce925_clk_y1_set_rate(struct clk_hw *hw, unsigned long rate,
    		unsigned long parent_rate)
    {
    	struct clk_cdce925_output *data = to_clk_cdce925_output(hw);
    
    	data->pdiv = cdce925_y1_calc_divider(rate, parent_rate);
    
    	return 0;
    }
    
    static const struct clk_ops cdce925_clk_y1_ops = {
    	.prepare = cdce925_clk_prepare,
    	.unprepare = cdce925_clk_unprepare,
    	.recalc_rate = cdce925_clk_recalc_rate,
    	.round_rate = cdce925_clk_y1_round_rate,
    	.set_rate = cdce925_clk_y1_set_rate,
    };
    
    #define CDCE925_I2C_COMMAND_BLOCK_TRANSFER	0x00
    #define CDCE925_I2C_COMMAND_BYTE_TRANSFER	0x80
    
    static int cdce925_regmap_i2c_write(
    	void *context, const void *data, size_t count)
    {
    	struct device *dev = context;
    	struct i2c_client *i2c = to_i2c_client(dev);
    	int ret;
    	u8 reg_data[2];
    
    	if (count != 2)
    		return -ENOTSUPP;
    
    	/* First byte is command code */
    	reg_data[0] = CDCE925_I2C_COMMAND_BYTE_TRANSFER | ((u8 *)data)[0];
    	reg_data[1] = ((u8 *)data)[1];
    
    	dev_dbg(&i2c->dev, "%s(%zu) %#x %#x\n", __func__, count,
    			reg_data[0], reg_data[1]);
    
    	ret = i2c_master_send(i2c, reg_data, count);
    	if (likely(ret == count))
    		return 0;
    	else if (ret < 0)
    		return ret;
    	else
    		return -EIO;
    }
    
    static int cdce925_regmap_i2c_read(void *context,
    	   const void *reg, size_t reg_size, void *val, size_t val_size)
    {
    	struct device *dev = context;
    	struct i2c_client *i2c = to_i2c_client(dev);
    	struct i2c_msg xfer[2];
    	int ret;
    	u8 reg_data[2];
    
    	if (reg_size != 1)
    		return -ENOTSUPP;
    
    	xfer[0].addr = i2c->addr;
    	xfer[0].flags = 0;
    	xfer[0].buf = reg_data;
    	if (val_size == 1) {
    		reg_data[0] =
    			CDCE925_I2C_COMMAND_BYTE_TRANSFER | ((u8 *)reg)[0];
    		xfer[0].len = 1;
    	} else {
    		reg_data[0] =
    			CDCE925_I2C_COMMAND_BLOCK_TRANSFER | ((u8 *)reg)[0];
    		reg_data[1] = val_size;
    		xfer[0].len = 2;
    	}
    
    	xfer[1].addr = i2c->addr;
    	xfer[1].flags = I2C_M_RD;
    	xfer[1].len = val_size;
    	xfer[1].buf = val;
    
    	ret = i2c_transfer(i2c->adapter, xfer, 2);
    	if (likely(ret == 2)) {
    		dev_dbg(&i2c->dev, "%s(%zu, %zu) %#x %#x\n", __func__,
    				reg_size, val_size, reg_data[0], *((u8 *)val));
    		return 0;
    	} else if (ret < 0)
    		return ret;
    	else
    		return -EIO;
    }
    
    static struct clk_hw *
    of_clk_cdce925_get(struct of_phandle_args *clkspec, void *_data)
    {
    	struct clk_cdce925_chip *data = _data;
    	unsigned int idx = clkspec->args[0];
    
    	if (idx >= ARRAY_SIZE(data->clk)) {
    		pr_err("%s: invalid index %u\n", __func__, idx);
    		return ERR_PTR(-EINVAL);
    	}
    
    	return &data->clk[idx].hw;
    }
    
    /* The CDCE925 uses a funky way to read/write registers. Bulk mode is
     * just weird, so just use the single byte mode exclusively. */
    static struct regmap_bus regmap_cdce925_bus = {
    	.write = cdce925_regmap_i2c_write,
    	.read = cdce925_regmap_i2c_read,
    };
    
    static int cdce925_probe(struct i2c_client *client,
    		const struct i2c_device_id *id)
    {
    	struct clk_cdce925_chip *data;
    	struct device_node *node = client->dev.of_node;
    	const char *parent_name;
    	const char *pll_clk_name[MAX_NUMBER_OF_PLLS] = {NULL,};
    	struct clk_init_data init;
    	u32 value;
    	int i;
    	int err;
    	struct device_node *np_output;
    	char child_name[6];
    	struct regmap_config config = {
    		.name = "configuration0",
    		.reg_bits = 8,
    		.val_bits = 8,
    		.cache_type = REGCACHE_RBTREE,
    	};
            printk("clock test ...................!!!!!!!!!!!!!!!!!!!!!\n");
    	dev_dbg(&client->dev, "%s\n", __func__);
    	data = devm_kzalloc(&client->dev, sizeof(*data), GFP_KERNEL);
    	if (!data)
    		return -ENOMEM;
    
    	data->i2c_client = client;
    	data->chip_info = &clk_cdce925_chip_info_tbl[id->driver_data];
            printk("number of PLL------------------------- %d",data->chip_info->num_plls);
    	config.max_register = CDCE925_OFFSET_PLL +
    		data->chip_info->num_plls * 0x10 - 1;
    	data->regmap = devm_regmap_init(&client->dev, &regmap_cdce925_bus,
    			&client->dev, &config);
    	if (IS_ERR(data->regmap)) {
    		dev_err(&client->dev, "failed to allocate register map\n");
    		return PTR_ERR(data->regmap);
    	}
    	i2c_set_clientdata(client, data);
    
    	parent_name = of_clk_get_parent_name(node, 0);
            printk("Parent name = %s\n", parent_name);
    	if (!parent_name) {
    		dev_err(&client->dev, "missing parent clock\n");
    		return -ENODEV;
    	}
    	dev_dbg(&client->dev, "parent is: %s\n", parent_name);
    
    	if (of_property_read_u32(node, "xtal-load-pf", &value) == 0)
    		regmap_write(data->regmap,
    			CDCE925_REG_XCSEL, (value << 3) & 0xF8);
    	/* PWDN bit */
    	regmap_update_bits(data->regmap, CDCE925_REG_GLOBAL1, BIT(4), 0);
    
    	/* Set input source for Y1 to be the XTAL */
    	regmap_update_bits(data->regmap, 0x02, BIT(7), 0);
    
    	init.ops = &cdce925_pll_ops;
    	init.flags = 0;
    	init.parent_names = &parent_name;
    	init.num_parents = parent_name ? 1 : 0;
    
    	/* Register PLL clocks */
    	for (i = 0; i < data->chip_info->num_plls; ++i) {
    		pll_clk_name[i] = kasprintf(GFP_KERNEL, "%s.pll%d",
    			client->dev.of_node->name, i);
    		init.name = pll_clk_name[i];
    		data->pll[i].chip = data;
    		data->pll[i].hw.init = &init;
    		data->pll[i].index = i;
    		err = devm_clk_hw_register(&client->dev, &data->pll[i].hw);
                    printk(" devm_clk_hw_register %d\n",err);
    		if (err) {
    			dev_err(&client->dev, "Failed register PLL %d\n", i);
    			goto error;
    		}
    		sprintf(child_name, "PLL%d", i+1);
                    
                    printk( "child name %s\n", child_name);
    		np_output = of_get_child_by_name(node, child_name);
    		if (!np_output)
    			continue;
                    value = 0;
                    printk( "after continue\n");
    		if (!of_property_read_u32(np_output,
    			"clock-frequency", &value)) {
    			err = clk_set_rate(data->pll[i].hw.clk, value);
                            printk("err =============%d\n" , err);
    			if (err)
    				dev_err(&client->dev,
    					"unable to set PLL frequency %ud\n",
    					value);
    printk("set frequency value = %ud\n", value);
    
    		}
    
    printk("1111 set frequency value = %d\n", value);
    		if (!of_property_read_u32(np_output,
    			"spread-spectrum", &value)) {
    			u8 flag = of_property_read_bool(np_output,
    				"spread-spectrum-center") ? 0x80 : 0x00;
    			regmap_update_bits(data->regmap,
    				0x16 + (i*CDCE925_OFFSET_PLL),
    				0x80, flag);
    			regmap_update_bits(data->regmap,
    				0x12 + (i*CDCE925_OFFSET_PLL),
    				0x07, value & 0x07);
    		}
    	}
    
    	/* Register output clock Y1 */
    	init.ops = &cdce925_clk_y1_ops;
    	init.flags = 0;
    	init.num_parents = 1;
    	init.parent_names = &parent_name; /* Mux Y1 to input */
    	init.name = kasprintf(GFP_KERNEL, "%s.Y1", client->dev.of_node->name);
    	data->clk[0].chip = data;
    	data->clk[0].hw.init = &init;
    	data->clk[0].index = 0;
    	data->clk[0].pdiv = 1;
    	err = devm_clk_hw_register(&client->dev, &data->clk[0].hw);
            printk("devm_clk_hw_register %d\n" , err);
    	kfree(init.name); /* clock framework made a copy of the name */
    	if (err) {
    		dev_err(&client->dev, "clock registration Y1 failed\n");
    		goto error;
    	}
    printk("number of outputs----------%d\n", data->chip_info->num_outputs);
    	/* Register output clocks Y2 .. Y5*/
    	init.ops = &cdce925_clk_ops;
    	init.flags = CLK_SET_RATE_PARENT;
    	init.num_parents = 1;
    	for (i = 1; i < data->chip_info->num_outputs; ++i) {
    		init.name = kasprintf(GFP_KERNEL, "%s.Y%d",
    			client->dev.of_node->name, i+1);
    		data->clk[i].chip = data;
    		data->clk[i].hw.init = &init;
    		data->clk[i].index = i;
    		data->clk[i].pdiv = 1;
    		switch (i) {
    		case 1:
    		case 2:
    			/* Mux Y2/3 to PLL1 */
                           
    			init.parent_names = &pll_clk_name[0];
                            printk("parent name = %s\n", pll_clk_name[0]);
    			break;
    		case 3:
    		case 4:
    
    			/* Mux Y4/5 to PLL2 */
    			init.parent_names = &pll_clk_name[1];
    			break;
    		case 5:
    		case 6:
    
    			/* Mux Y6/7 to PLL3 */
    			init.parent_names = &pll_clk_name[2];
    			break;
    		case 7:
    		case 8:
    
    			/* Mux Y8/9 to PLL4 */
    			init.parent_names = &pll_clk_name[3];
    			break;
    		}
    		err = devm_clk_hw_register(&client->dev, &data->clk[i].hw);
                    printk("devm_clk_hw_register %d\n" , err);
    		kfree(init.name); /* clock framework made a copy of the name */
    		if (err) {
    			dev_err(&client->dev, "clock registration failed\n");
    			goto error;
    		}
    	}
    
    	/* Register the output clocks */
    	err = of_clk_add_hw_provider(client->dev.of_node, of_clk_cdce925_get,
    				  data);
            printk("of_clk_add_hw_provider %d\n" , err);
    	if (err)
    		dev_err(&client->dev, "unable to add OF clock provider\n");
    
    	err = 0;
    
    error:
    	for (i = 0; i < data->chip_info->num_plls; ++i)
    		/* clock framework made a copy of the name */
    		kfree(pll_clk_name[i]);
    
    	return err;
    }
    
    static const struct i2c_device_id cdce925_id[] = {
    	{ "cdce913", CDCE913 },
    	{ "cdce925", CDCE925 },
    	{ "cdce937", CDCE937 },
    	{ "cdce949", CDCE949 },
    	{ }
    };
    MODULE_DEVICE_TABLE(i2c, cdce925_id);
    
    static const struct of_device_id clk_cdce925_of_match[] = {
    	{ .compatible = "ti,cdce913" },
    	{ .compatible = "ti,cdce925" },
    	{ .compatible = "ti,cdce937" },
    	{ .compatible = "ti,cdce949" },
    	{ },
    };
    MODULE_DEVICE_TABLE(of, clk_cdce925_of_match);
    
    static struct i2c_driver cdce925_driver = {
    	.driver = {
    		.name = "cdce925",
    		.of_match_table = of_match_ptr(clk_cdce925_of_match),
    	},
    	.probe		= cdce925_probe,
    	.id_table	= cdce925_id,
    };
    module_i2c_driver(cdce925_driver);
    
    MODULE_AUTHOR("Mike Looijmans <mike.looijmans@topic.nl>");
    MODULE_DESCRIPTION("TI CDCE913/925/937/949 driver");
    MODULE_LICENSE("GPL");
    

    It is mentioned that clk-cdce925.c is compatible with CDCE913 chip. But After booting when I probe the clock I am getting 25Mhz which is the default value.

    I am not sure whether  clk-cdce925.c is configuring the CDCE913 chip or not.

    Below is my device tree entry:

    cdce925@65 {
    #clock-cells = <1>;
    clocks = <&xtal>;
    compatible = "ti,cdce913";
    reg = <0x65>;
    ti,input-clock-type = "xtal";
    clock-names = "ref"; 
    clock-output-names = "pll", "pll-switched";
    PLL1 {
    spread-spectrum = <4>;
    clock-frequency = <100000000>, <100000000>, <100000000>;
    spread-spectrum-center;
    };

    xtal: xtal {
    #clock-cells = <0>;
    compatible = "fixed-clock";
    clock-frequency = <25000000>;
    clock-output-names = "xtal";
    };
    };

    Now my question is

    Why CDCE913 chip is not getting configured with clk-cdce925.c? Anything I am missing in my device tree entry?

    Please suggest.

    Thanks and Regards,

    Mahima Shanbag 

  • These codes are not developed by TI. Maybe cdce925.c original design target is to match all listed devices, but finally only implement cdce925.

    They are different devices

    – CDCE913/CDCEL913: 1-PLL, 3 Outputs
    – CDCE925/CDCEL925: 2-PLL, 5 Outputs