This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05028: LMK05028 power supply requirement

Part Number: LMK05028

Hi Team,

Dose LMK05028 has special requirement for bias power? such as ripple, noise...

Could you share the details power spec if it has

Thanks.

Oliver Ou

  • 1, Use a low-noise, high-PSRR LDO regulator to power the external oscillators used to drive the XO and TCXO
    inputs. Typically, oscillator jitter performance is typically impacted by switching noise on its power supply.

    2,

    Power supply Filtering is used to
    .Reduce the noise on the power supply rail from entering the sensitive blocks
    .Maximize isolation between circuitries on the same device

    Multiple VDDO pins can share a filtered supply when OUTs are the same frequency.

    Choose FB with some DCR
    .Reduces Q of LC filter, ZAC . 220 ohm @ 100 MHz, and DC current rating >2x above expected max current
    .Consider small damping resistor in series with large cap to mitigate LC resonant peaking

    Add multiple bypass cap value(s) to filter other known noise frequencies, especially if in the noise bandwidth of interest.

    3, LMK05028 internal LDOs also have some noise suppression. If clock jitter/phase noise is sensitive in user's application, a low noise, high-PSRR LDO with enough current capability is recommended, like XO supply.