Dear TI Community Team,
Please provide the below thermal parameter values of LMX2541SQ2690E part
ӨJA (°C/W) =?
ӨJC (°C/W) =?
ӨJB (°C/W) =?
TJ('C) =?
Thanks & regards,
Divya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Divya,
This is an older device and we don't have these values.
That being said, the current consumption is lower and we can estimate it.
The LMX2581 is a 32 pin package and has theta-ja=30 C/W and theta J-case=4 C/W
The LMX2594 is a 40 pin package and has theta ja=30 C/W and theta J-case = 0.9 C/W
So if you are operating about 170 mA at 3.3 V, this is about 0.5W
So if we ignore the theta J-Case and all other thermals, this would give a pessimistic increase of 15C.
WIth the Theta-J-Case, I think the increase would be much less. There is a metal DAP on the bottom to dissipate heat.
So I think that thermal should not be that much of a concern.
Regards,
Dean