This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208: About AC coupled VCM

Part Number: CDCM6208


Hi,

Our customers have questions about VCM for LVDS OUTPUT.
According to D / S, AC coupling VCM = VDD-0.76V (P14 6.17 LVDS (Low-Power CML) Output Characteristics).
If AC coupling is not used, the internal 50Ω pull-up of each differential output can be considered as 100Ω differential.
Looking at Figure 12, we can understand this.
Is it correct?
The actual measurement is the same.

I have one more question.
The output circuit is CML. Why is it VCM= VDD-0.76V?
They asked this question because simulating with commonly known CML circuits does not result in this VCM.

Best regard,
Hiroshi