Part Number: LMK04616
Hello,
I want to use the LMK04616 in single PLL2 mode as described in data sheet Figure 52, with CLKin0 = 100 MHz and CLKoutX 1GHz:n (with n = 1, 2, 4, 8)
With my current initialization I do not have PLL2 locked. (PLL2 VCO is ~7 GHz)
lmk04616 write 0000 99
lmk04616 write 008d 80
lmk04616 write 0015 00
lmk04616 write 0016 08
lmk04616 write 0017 14
lmk04616 write 0018 00
lmk04616 write 0019 00
lmk04616 write 001A 00
lmk04616 write 001B 00
lmk04616 write 001C 01
lmk04616 write 006C 01
lmk04616 write 006D 4c
lmk04616 write 006E 1B
lmk04616write 0146 30
lmk04616 write 0073 00
lmk04616 write 0074 0A
lmk04616 write 0075 00
lmk04616write 0076 00
lmk04616 write 0094 02
lmk04616 write 0095 13
lmk04616 write 0096 27
lmk04616 write 0010 1E
lmk04616 write 0011 01
What is missing/wrong ?
Regards