Hello,
is there any data on input impedance on the reference oscillator input and output impedance on the RF outputs?
The datasheet (section 7.3.1) simply says the input is high impedance but I see no value given - can I stick the output of a TCXO straight in with just an AC coupling cap or does it need some kind of matching network here?
Same issue at the RF output. Datasheet (section 7.3.7) just says output impedance is very small (how small?) and can be used to drive a 50R load. Can I take the output of the buffer and drive a 50 Ohm line (via AC coupling cap) or do I need some kind of match here? And does it matter whether I drive it single-ended or differential? I've had problems with inter-stage coupling before, and I really want to make sure I have this set up properly before commiting to using it in a design.
Thanks,
Gordon.