Can lmx2594 frequency synthesizer generate FMCW? Why is there an interval between the chip data display signals
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi There,
If the frequency ramp (or freq sweep) range is around 100MHz, LMX supports linear ramp - the so-called FMCW.
However, if the ramp range is very big, then the VCO will take some time to calibration itself to the correct frequency and therefore the freq ramp becomes a staircase ramp.
Hi There,
If VCO calibration is required during frequency ramping, we called it automatic ramp.
In the datasheet, Table 16 outlines all the necessary registers for automatic ramp, and there is an example in section 7.3.13.2.1.
You may also read LMX2572 datasheet section 8.1.7.2 for additional details on frequency ramping operation.