Part Number: LMK04610
Hi,
We have input frequencies 320 MHz and 450 MHz. How we should set doubler and dividers if we want to use Pll2 ? or we can only use bypass mode for those frequencies ?
Thank you,
Thiri
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04610
Hi,
We have input frequencies 320 MHz and 450 MHz. How we should set doubler and dividers if we want to use Pll2 ? or we can only use bypass mode for those frequencies ?
Thank you,
Thiri
Hello,
For PLL2 it can accept up to 600MHz input if driven differentially with the PLL2 REF clock divider selected.
The dividers should be set up so the PLL2 phase detector frequency is less than 250 MHz.
Regards,