Part Number: LMX2572
The datasheet makes a statement that "In general, the best performance is for a high slew rate but a lower amplitude signal, such as LVDS." How much of a difference does the amplitude make?
I'm using a buffer to drive the clock to it which is available with both LVDS and LVPECL outputs, but this presents a conundrum as the LVDS flavor of the part has worse jitter performance than the LVPECL. Without knowing how the LMX2572 reacts, I have no way to quantify what would give me better system performance (short of putting together some EVMs in the lab, but that's not really feasible).
Is there any data available that might quantify the "lower amplitude" statement? The LVPECL version of my buffer is about 90fs jitter 12k-20MHz (for my 100MHz reference), while the LVDS version is 107fs. While not a gigantic difference, it still is 17%. Given my loop bandwidth, the higher part of that curve doesn't matter, but the ~6dB differences from 10Hz to 1kHz offsets does.