Part Number: LMK00804B-Q1
Other Parts Discussed in Thread: LMK00804B, AWR1243
Hello,
I have couple of questions on LMK00804B-Q1.
First thing is, will this drive 50 ohm load? if yes then what is the VOH and VOL levels?
I'm using this in AWR1243, for Clock as per the reference design of cascaded AWR1243. My Question here is, LMK0084B has PU and PD on CLKn pin but for CLK pin it has only PD. I'm directly connecting output of AWR1243 OSC_CLKOUT to CLK pin of AWR1243 and CLKn I have added the voltage divider which gives 0.7V at CLKn pin. 33.2 Ohm in series, and trace impedance is 50Ohm. One of LMK00804B output is used in another Board through SMA. Here due to mismatch of voltage reference in CLK and CLKn pin, will their be any issues with duty cycle? Attaching my Circuit snapshot for your reference.
Regards,
Vinayak