This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592: Phase Synchronization

Part Number: LMX2592
Other Parts Discussed in Thread: LMX2594

We are using LMX2592 under following condition

  CHDIV=1 (VCO frequency=RFout frequency, 6GHz)

  Fractional 4th

  OSCin-Doubler, Pre-R-Divider, Multipler : not use

  Post-R-Divider: 1 (Input Signal frequency=Phase detector frequency, 80MHz)

If phase synchronization of multiple chips is required, do we need to use LMX2594?

Can LMX2592 guarantee phase synchronization in integer mode?

We want to avoid to change PLL-IC if possible.
  CHDIV=1 (VCO frequency=RFout frequency, 6GHz)

  Integer

  OSCin Doubler, Pre-R Divider, Multipler : not use

  Post-R Divider: 8 (80MHz=>10MHz)