Part Number: LM555
Other Parts Discussed in Thread: LM3886, TMUX6119, , CD4024B, TPA3116D2, UAF42
I am designing a circuit as part of my research on alternative strategies for overcoming cancer. The design consists of two oscillating circuits (already designed using programmable crystals and ripple-counters) producing the main frequency and a lower harmonic at typically 1.58 volts DC output. These are then passed through UAF42: Band Pass Filters to convert into sine-waves, the design of which has been so kindly created for me by kai klaas69. The outputs would then pass through an LM3886 amplifier to an impedance of 175 to 200 ohms.
The aim is to switch from one frequency to another at an interval of 5 minutes continuously. I am proposing that the Band Pass Filters are powered continuously from a parallel +/- 15volt supply. The two oscillator circuits are switched on at 5-minute intervals using a combination of a TMUX6119 switch controlled via an Astable LM555 circuit. The output from LM555 would go to SEL Pin8 on the TMUX6119, the 15 volts + supply would go to D Pin6, the 15 volts + output to the low-frequency circuit would be connected to SB Pin5 and the 15 volts + output to the high-frequency circuit would go to SA Pin 8.
As my knowledge of electronics is very limited, I would be extremely grateful if it was possible to evaluate the values of Ra Rb and Rl for the LM555, please? I also assume that the ouput from LM555 is at Pin3?
Thank you so very, very much.
CJJ