Other Parts Discussed in Thread: LMX2594,
It appears I am using the same board (based on the schematic screenshot in the referenced post) and am unable to use dual loop mode. It appears we have significant Jitter on our RFSOC DAC output, which we believe to be related to the reference clocks.
This part is being configured in single loop mode as in the attached tics file.
Additionally this part feeds a pair of LMX2594 devices which is then used to provide a 3.93216 GHz reference clock to the RFSOC DAC tiles. The configuration tics file of these devices is also attached.
Are there any suggestions to our configuration to improve clock jitter performance? Unfortunately we are unable to revise/rework 3rd party circuit board to include the mentioned .1uF Cap on the OSC_N pin.
Thankslmk04832.tcslmx2594.tcs