Hi,
I am using a 4DSP FMC120 board have LMK04828 as clock distribution.
Now I am trying to sync multiple this board by a external clock and sysref generator.
From the external clock and sysref generator, I generate 1G and 1G/256=3.9M signal connected to clock 1 (1G) and clock 0 (3.9M) of the LMK04828.
I use the attached registers (config1_output2_122M.txt) setting give me strange output on output 2, which should be 1G/4=250M but I got 122M, while the output 3 seems right which gave me the 3.9M from clock 0
If I then disable the sync_en as (config1_output2_252M.txt) and then of course I don't have the output 3 which should come from sysref.
How should I setup the chip to get the output 2 at 250M (clkin1/4) and output 3 at 3.9M (clkin0)?
Thanks,