Other Parts Discussed in Thread: LMX2531, LMX2572, LMX2582
Hi,
I'm a little new to the LMX2572LP series of synthesizers and would like to know what is the best way to begin designing with these parts other than goinf trough the datsheets etc. I notice there are various software packages to assist in this task but there seem to be three or so ... So which ones are recommended to start with.
Also it may be that the LMX2572LP, even though it appears to meet the requirements for low phase noise, it may not be the lowest power of them all. So was wondering if other similar parts may do as well with lower power consumption ? any suggestions right of the bat ?
With regards to choice of TCXO reference is an LVDS source recommended or will a standard TCXO sinfle-ended output be ok ? The application is for DMR in the ISM 868 and ISM 915 bands.
Will the simulation software be able to assist me with the choice of best reference input frequency (TCXO) for optimal phase noise and spurs at the 800 to 1GHz frequency band ? Otherwise whta method is recommended for this choice ??
regards,
mike