Part Number: TPL5010
Hello,
I am using TPL5010 to rest my microcontroller at certain period, but I come up with an issue. Following is the problem I have:
1. I am using battery to power both TPL5010 and the microcontroller.
2. I am using RST pin to reset the microntroller in case that the program is frozen. I could not use the watch dog in the microcontroller, because our board might go frozen by ESD and no program is running. The microcontroller can only be rest by pulling down the rest pin in that scenario.
3. However, when the battery is used up and I plug to charge the battery. The RST pin on TPL5010 is always low, and as a result the microcontroller cannot be turned on.
I was wondering whether anyone else has come up with the same issue. Any help is appreciated.
Thanks in advance.