Hello,
i'm using FSK bit mode for the LMX2571. There is a statement in the Manual about bit FSK_EN in register 24: "Enables FSK operation in all FSK operation modes. When this
bit is set, fractional denominator DEN should be zero." We can't use DEN=0 because we use big frequency deviation 360 kHz. Is it safe to use DEN not zero?
Thanks,
Alex