Part Number: LMX2571
Hello,
I'm using FSK I2S for the LMX2571. If the oversampling FSK modulation is used, what the maximum sampling rate can be achieved? in other words, what is the inertia of the FSK modulator?
Thanks,
Alex
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2571
Hello,
I'm using FSK I2S for the LMX2571. If the oversampling FSK modulation is used, what the maximum sampling rate can be achieved? in other words, what is the inertia of the FSK modulator?
Thanks,
Alex
Hi Alex,
Theoretically speaking, this is limited by the max. I2S clock rate, which is 100MHz.
However, there are couples of consideration for the chosen sampling rate. For example, loop filter bandwidth and spurs.
The following appnote has some suggestions.