This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LMX2595: lmx2595

Part Number: LMX2595

Tool/software: Code Composer Studio

Hello Sir/Ma'am

I want some data about the LMX2595 which I think it is missing in Datasheet.

In the data sheet see the 6.6 Section i.e. timing requirements

DIGITAL INTERFACE WRITE SPECIFICATIONS

fSPIWrite       SPI write speed       tCWL + tCWH > 13.333 ns      75 MHz

This 75MHz is the max. value.....will you please provide the min. and NOM value of fSPIWrite