Part Number: CDCLVD1212
Hi,
Is clipped sine wave input support CDCL 1212 2:12 buffer ic?. If you have any other option, please suggest.
Requirement - 2:12 10Mhz ,Input type- clipped sine wave.
Thank you
Anoop Varma m
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCLVD1212
Hi,
Is clipped sine wave input support CDCL 1212 2:12 buffer ic?. If you have any other option, please suggest.
Requirement - 2:12 10Mhz ,Input type- clipped sine wave.
Thank you
Anoop Varma m
Hi Anoop,
CDCLVD1212 can support a clipped sine input provided that it meets the requirements of the input characteristics in table 6.5 . Note that sine inputs would generally have slower edge rates than a square wave at the same frequency, which degrades the additive jitter performance. Clipped sine has faster edge rate than sine, but please verify that the performance will meet your requirements.
Kind regards,
Lane