On a small number of our boards (maybe 1%) a small proportion of times (<1%) after power-up the output of PLL2 is at half speed (74 MHz). Can you suggest what may be causing this to happen.
We are not currently using the I2C interface to control the device but instead depend on its default values.
The other PLL outputs are as we expect (#1 at 27MHz, #3 at 148, #4 at 24).
If I do use the I2C interface I can see that register 5 is at its default value of 0x2B, which should be forcing PLL2 to be 148.5MHz.
Probing the board we cannot see any excessive noise.
Cbpy2 sits at about 2.7V
Regards,
James.