Part Number: LMX2582
Hello,
In the TICS software, the description of Register 0 (specifically the Reset pin) says that when the device is reset, the registers are programmed to default values. I've read on other threads that it is required to program ALL registers on the initial programming sequence.
1.) Is this true?
2) If some registers are only going to be programmed to the default values (and reset "Resets" to the default values) why do I then need to re-program all of the registers?
assuming the answer to question 1 is true: is it required to program the registers in reverse order? R64-R0.
Thanks!
Tucker