This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVP111-SP: Maximum skew

Part Number: CDCLVP111-SP

The data sheet specifies the typical part-to-part skew.  What is the maximum part-to-part skew?

  • Hello Michael,

    Unfortunately we cannot guarantee a maximum specification for the part-to-part skew as we do not compare this across all the parts over temperature. However, we do test output to output skew and the datasheet lists the maximum on that.

    From the data I have it looks like the maximum difference I see over 50 parts is about 85 ps.

    Keep in mind this data is based on VCM = 1 V, VID = 0.5 V and FIN = 1 GHz.

    Thanks,

    Vibhu