This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: Phase-locking of LMX2595 synthesizer boards

Part Number: LMX2595

I would like to use two/one synthesizer boards as phase-locked source of a 6 and 18 GHz signal.

What is the best way to achieve this goal, while minimizing fluctuations?
Do I have to produce a SYSREF output at one device output that I use as SYNC input at the other?
What is the recommended setup for this application?

PS: I have a 100 MHz signal from a signal generator serving as input for both devices.