Part Number: LMK05028
Dear Sirs,
we are working on a new project where we want to get a PPS disciplined clock output from a TCXO, using the TI LMK05028.
Once configured LMK via i2c the, our custom board with LMK works as expected, except for the chip power consumption which is around 1.5W.
The chip overheats and the same goes for the whole pcb.
Is there a way to reduce the power consumption? We are not using the PLL1, only the PLL2.
Attached is a schematic of the LMK circuit and the .tcs file.
Best Regards,
Michele 7367.LMK.pdflmk.tcs