Hi team
Recently, I started to learn clock&timing products to support my customer, and I need your help to solve some basic questions. Thank you.
1. What is the function of Network Synchronizers?
"The LMK05318 is a high-performance network synchronizer clock device that provides jitter cleaning, clock generation, advanced clock monitoring, and superior hitless switching performance to meet the stringent timing requirements of communications infrastructure and industrial applications."
It seems that the network synchronizer is the high-level, rich-function product of jitter cleaner according to the description in the datasheet. Can you help briefly introduce the function of this kind of device?
2. What is the difference between the clock generator and the oscillator?
- As far as I know, these two devices both can generate the clock signals but the generator needs an external crystal.
- These two devices can be connected to a clock buffer to generate specific clock signals.
Look forward to your reply. Thank you.