Part Number: CDC7005-EVM
Other Parts Discussed in Thread: CDC7005
I do not have a direct PC->SPI interface connector, therefore, I am trying to use a MCU to program the CDC7005-EVM. The connection between my PC and the MCU is JTAG so I don't believe I can use the software supplied with the CDC7005-EVM because it uses SPI. Can you provide sample code to accomplish this, preferably in C, so I can use the code in Keil uVision5? I have a very vague understanding of how this would be accomplished based on CDC7005 data sheet. However, if the work could be narrowed down to just altering a few bits to change the various options provided in the software, that would make my job a whole lot simpler.