Part Number: CDCM61002
Other Parts Discussed in Thread: OMAP-L138
I am using 25MHz quartz crystal and strapped the chip configuration to output 100MHz CLK. The chip works as expected for a while but the issue seems to occur most if I recycle power to the chip after operating for a while then the output frequency changes from 100MHz to approximate 115MHz. Any idea of what may have caused this frequency change?
Note: Same behavior was captured on multiple units that uses the same configuration. Circuit is equivalent to the one used on the OMAP-L138 Development Board. http://www.ti.com/tool/TMDXLCDK138#technicaldocuments