I have a LMK04828 that is connected to an AD9690 ADC using LVDS. I inherited the design but I am a bit concerned regarding the LVDS levels. The datasheet states that the LMK diff output voltage is 395mV. But the ADC requires 600mV to 1.8V. Can someone confirm my fears that this wont work as it is? If so does anyone have good solution that I can use? Thanks