Part Number: LMX2615-SP
I have a customer interested using LMX2615-SP in a frequency agile application.
The output frequency range is 8250 to 10250 MHz in 5MHz steps. The reference frequency will be 100MHz.
The questions are as follows:
- What is the total time from the beginning of loading of the registers to a specified output frequency (including vco calibration and any other “housekeeping” functions that are necessary) to within 5 degrees settle tolerance? In other words, what would be the minimum time between any frequency jump?
- Are those frequencies in the range and spacing specified exact? Would there be any frequency error?
- If one were to use a 10MHz reference, what would be the minimum slew rate necessary for proper operation?
Thanks.