1)For a given CLKoutY output pair is configured for CMOS - Norm/Norm or Norm/Inv what is the state of the output pins when the respective CLKoutX_Y_PD bit is set?
2)For a given active CLKoutY output pair, configured for CMOS - Norm/Off or Inv/Off, what is teh state of the 'Off' output driver? ex high, low, ground, tristate
3) for CLKin0, used deferentially, and DC coupled, is there any data on where the input midpoint, or switching threshold is biased at (like VCC/2 on CMOS logic) for the MOS and Bipolar modes?